Skip to main content
DZimm.9
Associate III
November 11, 2019
Question

Debug multiple .elf files

  • November 11, 2019
  • 3 replies
  • 3073 views

Hello everyone

In one of our projects we created a bootloader and the application. Both projects are located in a separate workspace in the STMCubeIDE v1.10. My goal is to setup the GDB debugger in a way, that I can start the debugger from the bootloader and end up in the application. In this case, I could debug both projects at the same time.

Like most bootloaders is our bootloader checking if the version is correct and then jumps to the main applications start address. The memory location of the bootloader is defined in the linker script as:

/* Memories definition */
MEMORY
{
 CCMRAM	(xrw)	: ORIGIN = 0x10000000,	LENGTH = 64K
 SHAREDDATA (xrw) : ORIGIN = 0x20000000, LENGTH = 512
 RAM	(xrw)	: ORIGIN = 0x20000200,	LENGTH = 128K-512
 FLASH	(rx)	: ORIGIN = 0x8000000,	LENGTH = 16K-128 
 PRELOADERINFO (rx) : ORIGIN = 0x08003F80, LENGTH = 128
}

Whereas the application's memory is defined as:

/* Memories definition */
MEMORY
{
 PROGRAMINFO (rx) : ORIGIN = 0x08020000, LENGTH = 512 /* ProgramInfo and BootInfo */
 FLASH (rx) : ORIGIN = 0x08020200, LENGTH = 5*128K-512 /* Move APP to sector 5-9 */
 CCMRAM	(rwx)	: ORIGIN = 0x10000000,	LENGTH = 64K
 SHAREDDATA (xrw)	: ORIGIN = 0x20000000, LENGTH = 512
 RAM	(rwx)	: ORIGIN = 0x20000200,	LENGTH = 128K-512
}

I found several ways on how to setup multiple elf files (e.g. https://dzone.com/articles/multiple-binaries-with-gdbeclipse), but none of them really work...

What I found (but I'm not sure how to set this up) is an option under Run > Debug Configurations[Tab: Startup], where one can define multiple elf files. Upon launch, all the specified files are build and downloaded onto the CPU. Furthermore, the symbols are loaded from the elf file as well. Unfortunately, I haven't found any documentation about the offsets one need to specify.

There is a download and a symbol address offset which need to be defined.

For the download:

The offset is already taken from the linker script, therefore this offset should be 0, right?

For the symbol address:

Where can I get this offset? Using the .text offset doesn't really work. Once the debugger should jump the the applications code, only disassembly view is possible. My hope is to use the inline debugger for the main application as well.

I used readelf.exe to get an overview of the addresses and offsets:

There are 26 section headers, starting at offset 0x19101c:
 
Section Headers:
 [Nr] Name Type Addr Off Size ES Flg Lk Inf Al
 [ 0] NULL 00000000 000000 000000 00 0 0 0
 [ 1] .isr_vector PROGBITS 08020200 010200 000188 00 A 0 0 1
 [ 2] .text PROGBITS 08020388 010388 00e954 00 AX 0 0 8
 [ 3] .rodata PROGBITS 0802ecdc 01ecdc 0001a0 00 A 0 0 4
 [ 4] .programinfo PROGBITS 08020000 010000 000076 00 WA 0 0 4
 [ 5] .ARM.extab PROGBITS 0802ee7c 0204ac 000000 00 W 0 0 1
 [ 6] .ARM ARM_EXIDX 0802ee7c 01ee7c 000008 00 AL 2 0 4
 [ 7] .preinit_array PREINIT_ARRAY 0802ee84 0204ac 000000 04 WA 0 0 1
 [ 8] .init_array INIT_ARRAY 0802ee84 01ee84 000004 04 WA 0 0 4
 [ 9] .fini_array FINI_ARRAY 0802ee88 01ee88 000004 04 WA 0 0 4
 [10] .data PROGBITS 20000200 020200 0002ac 00 WA 0 0 4
 [11] .bss NOBITS 200004ac 0204ac 001564 00 WA 0 0 4
 [12] ._user_heap_stack NOBITS 20001a10 021a10 000600 00 WA 0 0 1
 [13] .ARM.attributes ARM_ATTRIBUTES 00000000 0204ac 000030 00 0 0 1
 [14] .debug_info PROGBITS 00000000 0204dc 0383ea 00 0 0 1
 [15] .debug_abbrev PROGBITS 00000000 0588c6 0055fd 00 0 0 1
 [16] .debug_aranges PROGBITS 00000000 05dec8 0019f0 00 0 0 8
 [17] .debug_ranges PROGBITS 00000000 05f8b8 0017a8 00 0 0 8
 [18] .debug_macro PROGBITS 00000000 061060 026f58 00 0 0 1
 [19] .debug_line PROGBITS 00000000 087fb8 01a315 00 0 0 1
 [20] .debug_str PROGBITS 00000000 0a22cd 0def19 01 MS 0 0 1
 [21] .comment PROGBITS 00000000 1811e6 00007b 01 MS 0 0 1
 [22] .debug_frame PROGBITS 00000000 181264 006f40 00 0 0 4
 [23] .symtab SYMTAB 00000000 1881a4 005aa0 10 24 849 4
 [24] .strtab STRTAB 00000000 18dc44 0032c0 00 0 0 1
 [25] .shstrtab STRTAB 00000000 190f04 000117 00 0 0 1
Key to Flags:
 W (write), A (alloc), X (execute), M (merge), S (strings), I (info),
 L (link order), O (extra OS processing required), G (group), T (TLS),
 C (compressed), x (unknown), o (OS specific), E (exclude),
 y (purecode), p (processor specific)

Does anyone have any experience in setting this IDE up for multiple elf files?

Thank you in advance and best regards

Daniel

This topic has been closed for replies.

3 replies

Maximilian Pohl
Associate III
March 17, 2023

any progress on that?

Tesla DeLorean
Guru
March 17, 2023

Other platforms you should be able to list the file(s) in a debugger script.

Do you need source to understand the code? In default operation Keil can have source behind one, but can debug code without any source code, so on the loader side you'd debug to the transition point, step on thru the transition, and however deep into the app you need to see it working/succeeding.

One might be able to merge .ELF files, not sure there's a specific commercial/off-the-shelf tools to do that, but I've built such tools in the past.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Pavel A.
March 17, 2023

@Maximilian Pohl​ Yes there is progress. Recent CubeIDE versions support importing an elf executable for debugging, maybe even ELFs made with non-gnu toolchain.

The CubeIDE debugger can also load multiple ELF executables, or only the debug symbols without rewriting the flash.

If the other projects are in other Eclipse workspace, you can temporarily import them into the active workspace.