Skip to main content
PPate.1029
Associate II
November 11, 2019
Question

Ethernet communication problem with NUCLEO-H743ZI

  • November 11, 2019
  • 2 replies
  • 647 views

Is there any simplified version of ETH just to transmit data in a way similar to HAL_UART_Transmit() function?

Can anyone provide the code for the same (sending and receiving packets using STM32H743) without/with using LWIP. Please recommend the software for testing the same.

This topic has been closed for replies.

2 replies

Tesla DeLorean
Guru
November 11, 2019

Like HAL_ETH_TransmitFrame() ?

Wireshark or network analyzer connected to different port of 10BT *HUB* ? Or another Ethernet node in promiscuous mode?

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
PPate.1029
Associate II
November 11, 2019

Like HAL_ETH_TransmitFrame() ? : Yes, is it possible using this function ?

Wireshark or network analyzer connected to different port of 10BT *HUB* ? : yes connected.

If you have a running example code, it is very helpful to me