Skip to main content
TOlli
Senior
November 7, 2019
Solved

H755ZI. Selected processor does not support 'isb 0xF' in ARM mode

  • November 7, 2019
  • 3 replies
  • 3527 views

Hi,

I'm trying to compile the BSP example project from the H7 FW package, and I keep getting these error messages:

Scanning dependencies of target Demo_M4_Single.elf
[ 4%] Building C object CMakeFiles/Demo_M4_Single.elf.dir/Drivers/STM32H7xx_HAL_Driver/Src/stm32h7xx_hal_cortex.c.obj
[ 9%] Building C object CMakeFiles/Demo_M4_Single.elf.dir/Drivers/STM32H7xx_HAL_Driver/Src/stm32h7xx_hal_flash.c.obj
[ 13%] Building C object CMakeFiles/Demo_M4_Single.elf.dir/Drivers/STM32H7xx_HAL_Driver/Src/stm32h7xx_hal_flash_ex.c.obj
[ 18%] Building C object CMakeFiles/Demo_M4_Single.elf.dir/Drivers/STM32H7xx_HAL_Driver/Src/stm32h7xx_hal_gpio.c.obj
C:\Users\ton\AppData\Local\Temp\ccxCvotZ.s: Assembler messages:
C:\Users\ton\AppData\Local\Temp\ccxCvotZ.s:118: Error: selected processor does not support `isb 0xF' in ARM mode
C:\Users\ton\AppData\Local\Temp\ccxCvotZ.s:129: Error: selected processor does not support `dsb 0xF' in ARM mode
C:\Users\ton\AppData\Local\Temp\ccxCvotZ.s:162: Error: selected processor does not support `isb 0xF' in ARM mode
C:\Users\ton\AppData\Local\Temp\ccxCvotZ.s:173: Error: selected processor does not support `dsb 0xF' in ARM mode
C:\Users\ton\AppData\Local\Temp\ccxCvotZ.s:360: Error: selected processor does not support `isb 0xF' in ARM mode
C:\Users\ton\AppData\Local\Temp\ccxCvotZ.s:371: Error: selected processor does not support `dsb 0xF' in ARM mode
C:\Users\ton\AppData\Local\Temp\ccxCvotZ.s:404: Error: selected processor does not support `isb 0xF' in ARM mode
C:\Users\ton\AppData\Local\Temp\ccxCvotZ.s:415: Error: selected processor does not support `dsb 0xF' in ARM mode
mingw32-make.exe[3]: *** [CMakeFiles/Demo_M4_Single.elf.dir/Drivers/STM32H7xx_HAL_Driver/Src/stm32h7xx_hal_flash.c.obj] Error 1
mingw32-make.exe[3]: *** Waiting for unfinished jobs....
CMakeFiles\Demo_M4_Single.elf.dir\build.make:165: recipe for target 'CMakeFiles/Demo_M4_Single.elf.dir/Drivers/STM32H7xx_HAL_Driver/Src/stm32h7xx_hal_flash.c.obj' failed
C:\Users\ton\AppData\Local\Temp\ccFiuVRY.s: Assembler messages:
C:\Users\ton\AppData\Local\Temp\ccFiuVRY.s:211: Error: selected processor does not support `dsb 0xF' in ARM mode
C:\Users\ton\AppData\Local\Temp\ccFiuVRY.s:222: Error: selected processor does not support `isb 0xF' in ARM mode
C:\Users\ton\AppData\Local\Temp\ccFiuVRY.s:773: Error: selected processor does not support `dsb 0xF' in ARM mode
C:\Users\ton\AppData\Local\Temp\ccFiuVRY.s:793: Error: selected processor does not support `dsb 0xF' in ARM mode
C:\Users\ton\AppData\Local\Temp\ccFiuVRY.s:1134: Error: selected processor does not support `dmb 0xF' in ARM mode
C:\Users\ton\AppData\Local\Temp\ccFiuVRY.s:1204: Error: selected processor does not support `dsb 0xF' in ARM mode
C:\Users\ton\AppData\Local\Temp\ccFiuVRY.s:1215: Error: selected processor does not support `isb 0xF' in ARM mode
CMakeFiles\Demo_M4_Single.elf.dir\build.make:139: recipe for target 'CMakeFiles/Demo_M4_Single.elf.dir/Drivers/STM32H7xx_HAL_Driver/Src/stm32h7xx_hal_cortex.c.obj' failed
mingw32-make.exe[3]: *** [CMakeFiles/Demo_M4_Single.elf.dir/Drivers/STM32H7xx_HAL_Driver/Src/stm32h7xx_hal_cortex.c.obj] Error 1
CMakeFiles\Makefile2:74: recipe for target 'CMakeFiles/Demo_M4_Single.elf.dir/all' failed
CMakeFiles\Makefile2:81: recipe for target 'CMakeFiles/Demo_M4_Single.elf.dir/rule' failed
mingw32-make.exe[2]: *** [CMakeFiles/Demo_M4_Single.elf.dir/all] Error 2
mingw32-make.exe[1]: *** [CMakeFiles/Demo_M4_Single.elf.dir/rule] Error 2
mingw32-make.exe: *** [Demo_M4_Single.elf] Error 2
Makefile:117: recipe for target 'Demo_M4_Single.elf' failed

I don't get these error messages when I'm using STM32CubeIDE, so there must be something off in my configuration. But I don't have any idea where to look for the answer, I know some of the commands are related to memory barriers in MPU and some are assembly commands for wait for interrupt (this one does not show above).

I have double checked the configurations etc (so I shouldn't missing any flags), but this still happens.

SET(CMAKE_SYSTEM_NAME Generic)
SET(CMAKE_SYSTEM_VERSION 1)
cmake_minimum_required(VERSION 3.15)
project(Demo_M4_Single C CXX ASM)
 
SET(TRUE 1)
SET(FALSE 0)
SET(LOCAL_ARM_TOOLCHAIN C:/GNU-Tools-Arm-Embedded/7-2018-q2-update)
SET(H7_FW_PATH C:/Users/ton/STM32Cube/Repository/STM32Cube_FW_H7_V1.5.0)
 
# Specify cross compilers and tools
SET(CMAKE_C_COMPILER_WORKS 1)
SET(CMAKE_C_COMPILER arm-none-eabi-gcc)
 
SET(CMAKE_CXX_COMPILER_WORKS 1)
SET(CMAKE_CXX_COMPILER arm-none-eabi-g++)
 
SET(CMAKE_ASM_COMPILER arm-none-eabi-gcc)
 
SET(CMAKE_AR arm-none-eabi-ar)
SET(CMAKE_OBJCOPY arm-none-eabi-objcopy)
SET(CMAKE_OBJDUMP arm-none-eabi-objdump)
SET(SIZE arm-none-eabi-size)
 
SET(linkerScript stm32h755xx_flash_CM4.ld)
SET(LINKER_SCRIPT ${CMAKE_SOURCE_DIR}/${linkerScript})
 
# Uncomment for hardware accelerated floating point calculation
SET(FPU_FLAGS "-mfloat-abi=hard -mfpu=fpv4-sp-d16")
add_definitions(-DARM_MATH_CM4 -DARM_MATH_MATRIX_CHECK -DARM_MATH_ROUNDING -D__FPU_PRESENT=1
 -DUSE_HAL_DRIVER
 -DSTM32H755xx # Defining the board
 -DCORE_CM4 # Define the Core we are buiding for
 -DUSE_STM32H7XX_NUCLEO_144_MB1363
 )
 
# Uncomment for software floating point calculation
#SET(FPU_FLAGS "-mfloat-abi=soft")
 
SET(COMMON_FLAGS
 "-mcpu=cortex-m4 ${FPU_FLAGS} -mthumb -mthumb-interwork -ffunction-sections -fdata-sections \
 -g -fno-common -fmessage-length=0 ${linkerFlags}")
 
SET(CMAKE_CXX_FLAGS_INIT "${COMMON_FLAGS} -std=c++11")
SET(CMAKE_C_FLAGS_INIT "${COMMON_FLAGS} -std=gnu11")
 
SET(CMAKE_EXE_LINKER_FLAGS_INIT "-Wl,-gc-sections,--print-memory-usage -T $${LINKER_SCRIPT}")
 
# Add resources files to the project
file(GLOB_RECURSE SOURCES
 #${PROJECT_SOURCE_DIR}/main.c
 ${PROJECT_SOURCE_DIR}/CM4/Src/*.*
 ${PROJECT_SOURCE_DIR}/Common/Src/*.*
 ${PROJECT_SOURCE_DIR}/Drivers/STM32H7xx_HAL_Driver/Src/*.*
 ${PROJECT_SOURCE_DIR}/startup/*.*
 )
 
# Include Directories to the project
include_directories(
 ${LOCAL_ARM_TOOLCHAIN}/arm-none-eabi/include
 ${H7_FW_PATH}/Drivers/BSP/Components/Common
 ${H7_FW_PATH}/Drivers/BSP/Components/st7735
 ${H7_FW_PATH}/Drivers/BSP/STM32H7xx_Nucleo_144
 ${H7_FW_PATH}/Drivers/CMSIS/Device/ST/STM32H7xx/Include
 ${H7_FW_PATH}/Drivers/CMSIS/Include
 ${H7_FW_PATH}/Drivers/STM32H7xx_HAL_Driver/Inc
 
 ${PROJECT_SOURCE_DIR}/CM4/Inc
 
 ${PROJECT_SOURCE_DIR}/Drivers/BSP/Adafruit_Shield/Inc
 ${PROJECT_SOURCE_DIR}/Drivers/BSP/Component/Inc
 ${PROJECT_SOURCE_DIR}/Drivers/BSP/STM32H7xx_Nucleo/Inc
 
 ${PROJECT_SOURCE_DIR}/Drivers/CMSIS/Inc
 
 ${PROJECT_SOURCE_DIR}/Drivers/STM32H7xx_HAL_Driver/Inc
)
 
# Make sure everything is compiled for the application
add_executable(${PROJECT_NAME}.elf ${SOURCES} ${LINKER_SCRIPT})
 
set(CMAKE_EXE_LINKER_FLAGS
 "${CMAKE_EXE_LINKER_FLAGS}} -Wl, -Map=${PROJECT_BINARY_DIR}/${PROJECT_NAME}.map")
 
SET_TARGET_PROPERTIES(${PROJECT_NAME}.elf PROPERTIES LINKER_LANGUAGE C)
 
set(HEX_FILE ${PROJECT_BINARY_DIR}/${PROJECT_NAME}.hex)
set(BIN_FILE ${PROJECT_BINARY_DIR}/${PROJECT_NAME}.obj)
 
add_custom_command(TARGET ${PROJECT_NAME}.elf POST_BUILD
 COMMAND ${CMAKE_OBJCOPY} -Oihex $<TARGET_FILE:${PROJECT_NAME}.elf> ${HEX_FILE}
 COMMAND ${CMAKE_OBJCOPY} -Oihex $<TARGET_FILE:${PROJECT_NAME}.elf> ${BIN_FILE}
 COMMENT "Building ${HEX_FILE} Building ${BIN_FILE}"
 )

Above is my CMake file if it helps. Other than that, I have just copied the exact same folder structure from the example project BSP to this one.

My system otherwise is as follows:

Windows 10

Clion 2019.2.5

MinGW 5.2 (as reported by CLion)

CMake 3.15.3 (bundled with CLion)

gcc --version outputs this: 8.2.0-3

I found a previous post that just updated their tool (SW4), but that is not really an option here.

Any ideas are appreciated.

Please and thank you,

Tero

This topic has been closed for replies.
Best answer by TOlli

Hi,

So I managed to solve the issue. The issue was in the CMakeLists.txt syntax I was using. I don't know for sure what was wrong with my variables (I defined variables for paths to keep them manageable), but when I deleted them, the rest of the file started to work correctly. I though I was doing the same as my other colleague in their projects but I guess not. Maybe I will get back to those at some other time.

The cross compilers I had to define through ENV-variables (CC, CXX, AMS), and after that, I managed to at least compile the M4 side of the example project.

Thanks everyone!

Hopefully this will be helpful for the next guy running into strange issues.

-Tero

3 replies

berendi
Principal
November 7, 2019

Something is definitely off with your config, because you write

gcc --version outputs this: 8.2.0-3

yet your CMakefile contains

SET(LOCAL_ARM_TOOLCHAIN C:/GNU-Tools-Arm-Embedded/7-2018-q2-update)

which should print something like this

/opt/gcc-arm-none-eabi-7-2018-q2-update/bin/arm-none-eabi-gcc --version
arm-none-eabi-gcc (GNU Tools for Arm Embedded Processors 7-2018-q2-update) 7.3.1 20180622 (release) [ARM/embedded-7-branch revision 261907]

TOlli
TOlliAuthor
Senior
November 8, 2019

Hello Berendi,

You are right. I was using the wrong command above, if I do

arm-none-eabi-gcc --version
arm-none-eabi-gcc (GNU Tools for Arm Embedded Processors 7-2018-q2-update) 7.3.1 20180622 (release) [ARM/embedded-7-branch revision 261907]

I was rechecking my Cmake logs and it seems that the tool doesn't (for some unknown reason for now) change to the arm toolchain as specified in the CMake-file, but tries to use the normal MinGW gcc and I'm guessing that is why I'm seeing the error messages as the target is now my windows 10 machine, which I assume does not have support for those commands.

Back to the drawing board, the problem must be in CLion and it's plugins that create the embedded project.

Best regards,

Tero

TOlli
TOlliAuthorBest answer
Senior
November 8, 2019

Hi,

So I managed to solve the issue. The issue was in the CMakeLists.txt syntax I was using. I don't know for sure what was wrong with my variables (I defined variables for paths to keep them manageable), but when I deleted them, the rest of the file started to work correctly. I though I was doing the same as my other colleague in their projects but I guess not. Maybe I will get back to those at some other time.

The cross compilers I had to define through ENV-variables (CC, CXX, AMS), and after that, I managed to at least compile the M4 side of the example project.

Thanks everyone!

Hopefully this will be helpful for the next guy running into strange issues.

-Tero