Question
Configuring I2S Clock (stm32h7)
Hello
I am trying to establish I2S communication with external audio codec. The manual says the I2S clock (Fi2s_clk) is a function of the audio frequency. There is table with example frequencies. For example, the table provides 3 examples for frequency Fws = 48kHz, and possible Fi2s_clk are 12.288MHz, 49.152MHz, and 61.44Mhz. I was not able to get such frequencies with the CubeMX application (i am using HSE=25Mhz).
How can I configure the audio communication if I cannot set the right input clock for the I2S?