Skip to main content
RMcCa
Senior II
November 7, 2019
Question

H745 MDMA document error? (RM0399)

  • November 7, 2019
  • 2 replies
  • 780 views

In 15.5.12, the register definition for mdma_ctbr , i am having trouble understanding the dbus and sbus bit descriptions. Shouldn't the choices be between tcm/axi and ahb/system and not system/axi and ahb/tcm as the latter is mixing the domains together and is thus meaningless?​ which is which? Wouldn't it be clearer if the choice was D1 or D2?

​

T​hanks.

This topic has been closed for replies.

2 replies

waclawek.jan
Super User
November 7, 2019

TCM is not in D1 nor D2 domain, it's an exception not going through the bus matrices but a dedicated interconnection between MDMA and the AHBS port of processor - and it's a 32-bit bus. So the description might rather be "64/32 bit" or "AXI/non-AXI".

JW

RMcCa
RMcCaAuthor
Senior II
November 7, 2019

Thank you for the clarification. In looking deeper into what i was doing, i realized it was wrong anyway. I was trying to use mdma and dma to get single char​s from uart5 to tcm which seemed weird and cumbersome. I have switched to using dma2 handled by the m4 core to store the incoming bytes in a ram3 buffer and using mdma memory to memory to copy the buffer to tcm. I already have the code to exchange data between the two cores via mdma, so i just changed it so that the rx data is copied to the m7 not from it.