Skip to main content
RMcCa
Senior II
Nov 6, 2019 2:34 PM UTC
Question

Configure DMA for MDMA H7 dual core

Sorry to be asking so many questions, but these dual core h7s are hella complicated and the documentation can be a little vague.

I am trying to understand how to set up the dmas to work with the mdma. I think i get the dmamux and how the mdma works with dma channels, but am unsure about the interrelationships between the mdma block size and the dma ​ntdr.

In one case, i am receiving 8 half words in a single burst from an spi in slave mode. Should i set the dma ntdr to 8 and the mdma block size also to 8 with a common 8 half word ahb ram buffer in between? I would like to use an mdma transfer complete interrupt in the f7 code to trigger when all 8 half words have been recieved & copied into tcm ram.

Also​, i have a 9600 baud uart rx for ascii hex command reception. I would like to set it up so that i can use the uart character match interrupt to stop the mdma and read the number of bytes recieved by the mdma from the uart dma channel. Should i set the dma ntdr to 1 and the mdma block size to the ram buffer size? The buffer is 256 bytes, which is plenty big enough for a command. If i initialize the mdma block size to 256, will i be able to simply read the count and subtract from 256 to get the message length in the uart character match isr? This works with an f7, setting ndtr to 256.

​

Thanks.​

This topic has been closed for replies.