What is the reason for compile errors with STM32CubeIDE for STEVAL-SPIN3201 and STEVAL-ESC001V1 sample programs that are unable to find modules even though the libraries with the "missing" modules are in the includes?
Compile error is:
make[1]: *** No rule to make target 'C:/Users/david/STM32CubeIDE/workspace_1.1.0/SPIN3201/SDK5x - STEVAL-SPIN3201 - BullRunning/Drivers/STM32F0xx_HAL_Driver/Src/stm32f0xx_hal_exti.c', needed by 'Drivers/STM32F0xx_HAL_Driver/stm32f0xx_hal_exti.o'. Stop. SDK5x - STEVAL-SPIN3201 - BullRunning C/C++ Problem
The missing file (stm32f0xx_hal_exti.c) is located in a directory that was included in the project properties, both in the PATH of the C/C++ Build Environment and the INCLUDES of the C/C++ General Paths and Symbols:
C:\Users\david\STM32Cube\Repository\STM32Cube_FW_F0_V1.11.0\Drivers\STM32F0xx_HAL_Driver\Src
But based on the error message, it seems it has not found the module. What is missing?
The process is using the Motor Control Workbench that calls STM32CubeMX that then opens the project in STM32CubeIDE with TrueSTUDIO Toolchain.