Question
STM32F411E-DISCO CubeMX's repository issue
Hello, I've find one hidden fail in template project for STM32F411E-DISCO (STM32Cube\Repository\STM32Cube_FW_F4_V1.24.1\Projects\STM32F411E-Discovery\Templates). In header file inc/stm32f4xx_hal_conf.h there is a wrong define of hse frequency:
#if !defined (HSE_VALUE)
#define HSE_VALUE ((uint16_t)8000000U) /*!< Value of the External oscillator in Hz */
#endif /* HSE_VALUE */8000000U it's not uin16_t, so it should be:
#if !defined (HSE_VALUE)
#define HSE_VALUE (8000000U) /*!< Value of the External oscillator in Hz */
#endif /* HSE_VALUE */I meet this, when I manually create new project from System Workbench for STM32 (New->C Project->Executable->Ac6 STM32 MCU Project...)...
STM32Cube_FW_F4_V1.24.1
CubeMX 5.4.0.
Hope this will be fixed and will help somebody.