Skip to main content
DevBee
Associate III
November 1, 2019
Question

Modifying tick period to 0.01 millisecond has no effect in generated code (default is 1 millisec or 1 KHz frequency) with TIM8 as Timebase source in System configuration.

Hi,

Am using STM32CubeIDE with FreeRTOS middleware (CMSISv1).

I dont see change in code generated in file stm32f4xx_hal_timebase_tim.c when I modify tick frequency to 100000 instead of the default 1000. In sys tab of configuration setting TIM8 as timebase source.

Below is the code in stm32f4xx_hal_timebase_tim.c :

HAL_StatusTypeDef HAL_InitTick(uint32_t TickPriority)

{

 RCC_ClkInitTypeDef   clkconfig;

 uint32_t             uwTimclock = 0;

 uint32_t             uwPrescalerValue = 0;

 uint32_t             pFLatency;

 /*Configure the TIM8 IRQ priority */

 HAL_NVIC_SetPriority(TIM8_UP_TIM13_IRQn, TickPriority ,0);

 /* Enable the TIM8 global Interrupt */

 HAL_NVIC_EnableIRQ(TIM8_UP_TIM13_IRQn);

 /* Enable TIM8 clock */

 __HAL_RCC_TIM8_CLK_ENABLE();

 /* Get clock configuration */

 HAL_RCC_GetClockConfig(&clkconfig, &pFLatency);

 /* Compute TIM8 clock */

 uwTimclock = 2*HAL_RCC_GetPCLK2Freq();

 /* Compute the prescaler value to have TIM8 counter clock equal to 1MHz */

 uwPrescalerValue = (uint32_t) ((uwTimclock / 1000000) - 1);

 /* Initialize TIM8 */

 htim8.Instance = TIM8;

 htim8.Init.Period = (1000000 / 1000) - 1;

 htim8.Init.Prescaler = uwPrescalerValue;

 htim8.Init.ClockDivision = 0;

 htim8.Init.CounterMode = TIM_COUNTERMODE_UP;

......

......

.....

}

Kindly confirm if my above understanding is correct ? Will this be done if I modify as below:

htim8.Init.Period = (1000000 - 1); // instead of ((1000000/1000) -1)

I have already set configTICK_RATE_HZ as 1000 in FreeRTOSConfig.h. What other modifications do I need to make?

Thank you.

This topic has been closed for replies.

1 reply

DevBee
DevBeeAuthor
Associate III
November 1, 2019

Checked the output on tracelyzer, and see the change working with respect to ticks, but still scheduling is not appropriate, so I need to make some more modifications in generated code. Kindly guide me.