Skip to main content
parisa
Associate III
November 1, 2019
Solved

SPI chip select pin

  • November 1, 2019
  • 6 replies
  • 2919 views

Hello,

I need to connect more than 2 MCUs with SPI connection(1 Master, 2Slaves). Here is my Hardware connections :

MISO1->MOSI2 && MOSI3

MOSI1->MISO2 && MISO3

SCK1->SCK2 && SCK3

NSS1->NSS2 && NSS3

But I don't know how I can select each slave with master (MCU1). Is there any SPI chip select available in the MCU or it i desired?

This topic has been closed for replies.
Best answer by S.Ma

If you have 2 slaves and it's a multi-drop bus, use 2 GPIOs on the master side and connect each one of them to the NSS of each slave.

Then you can use the HW NSS SPI function on slave side to disconnect MISO when NSS is high (unselected).

In my projects, I used a different scheme to have up to 12 SPI slaves with 6 pins in multidrop mode. This is another story, although all works fine without NSS HW setup, I use NSS as EXTI interrupt to disable MISO pin and it's working fine, while having the HW NSS option as fallback.

6 replies

TDK
November 1, 2019

Take out the NSS line. The hardware NSS signal is not useful.

Instead, hook up two CS lines as general GPIO pins from the master to slave. One line per slave. Hold those high by default and select a slave by pulling that line low during communication.

"If you feel a post has answered your question, please click ""Accept as Solution""."
S.Ma
Principal
November 1, 2019

If you have only 1 master and 1 slave, it's point to point, so yes, you don't need to bother with NSS on the slave side to put tristate MISO by NSS high level.

parisa
parisaAuthor
Associate III
November 1, 2019

Thank you for you comment.

In the 1master and 2 clients configuration should I use NSS pin?

parisa
parisaAuthor
Associate III
November 1, 2019

I really appreciate your explanation.

In the software, how can I implement this chip select pin? it means if the line is high I should ignore the incoming packets or there is another approach to implement in SPI software and it configures the software the CS pins.

S.Ma
S.MaBest answer
Principal
November 1, 2019

If you have 2 slaves and it's a multi-drop bus, use 2 GPIOs on the master side and connect each one of them to the NSS of each slave.

Then you can use the HW NSS SPI function on slave side to disconnect MISO when NSS is high (unselected).

In my projects, I used a different scheme to have up to 12 SPI slaves with 6 pins in multidrop mode. This is another story, although all works fine without NSS HW setup, I use NSS as EXTI interrupt to disable MISO pin and it's working fine, while having the HW NSS option as fallback.

Visitor II
February 26, 2025

Hi

Were you able to do this? Can you please help me :folded_hands:. Can you please share me the code or atleast the connections you implemented on the controllers? 

 

STM is so confusing and difficult. The useful resources are very low in STM32