Is it ok if uart communication of vcom_init () is rs-485? (vcom.c)
Hi
I use 'PRINTF' and 'AT command' using vcom.c from the I-CUBE-LRWAN source.
And develop in the following situations.
1. UART communication uses RS-232.
2. I use STM32L082 low-power chip.
3.I use LPUART and NVIC interrupts.
and then, I made the following changes and tested them.
1.change uart port. (usart2 - > usart1)
2.in usart1 port i uses RS-485.
Then PRINTF and AT-command do not work.
Do you have to add other parts to the following sources when using rs-485? Or can you use usart1 as the uart port of lpuart? (See terminal configuration)
void vcom_Init(void)
{
LL_LPUART_InitTypeDef LPUART_InitStruct;
/*## Configure the UART peripheral ######################################*/
/* Put the UART peripheral in the Asynchronous mode (UART Mode) */
/* UART1 configured as follow:
- Word Length = 8 Bits
- Stop Bit = One Stop bit
- Parity = ODD parity
- BaudRate = 921600 baud
- Hardware flow control disabled (RTS and CTS signals) */
/*
* Clock initialization:
* - LSE source selection
* - LPUART clock enable
* - GPIO clocks are enabled in vcom_IoInit()
*/
LL_RCC_SetLPUARTClockSource(LL_RCC_LPUART1_CLKSOURCE_HSI);
UARTX_CLK_ENABLE();
vcom_IoInit(); /* init vcom */
LPUART_InitStruct.BaudRate = 115200;
LPUART_InitStruct.DataWidth = LL_LPUART_DATAWIDTH_8B;
LPUART_InitStruct.StopBits = LL_LPUART_STOPBITS_1;
LPUART_InitStruct.Parity = LL_LPUART_PARITY_NONE;
LPUART_InitStruct.TransferDirection = LL_LPUART_DIRECTION_TX_RX;
LPUART_InitStruct.HardwareFlowControl = LL_LPUART_HWCONTROL_NONE;
if (LL_LPUART_Init(UARTX, &LPUART_InitStruct) != SUCCESS)
{
Error_Handler();
}
/* Configuring the LPUART specific LP feature - the wakeup from STOP */
LL_LPUART_EnableInStopMode(UARTX);
/* WakeUp from stop mode on start bit detection*/
LL_LPUART_SetWKUPType(UARTX, LL_LPUART_WAKEUP_ON_STARTBIT);
//LL_LPUART_SetWKUPType(UARTX, LL_LPUART_WAKEUP_ON_RXNE);
LL_LPUART_EnableIT_WKUP(UARTX);
LL_LPUART_Enable(UARTX);
while (LL_LPUART_IsActiveFlag_TEACK(UARTX) == RESET)
{
;
}
while (LL_LPUART_IsActiveFlag_REACK(UARTX) == RESET)
{
;
}
uart_context.gState = HAL_UART_STATE_READY;
uart_context.RxState = HAL_UART_STATE_READY;
}
void vcom_IoInit(void)
{
GPIO_InitTypeDef GPIO_InitStruct;
/* UART TX GPIO pin configuration */
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_MEDIUM;
GPIO_InitStruct.Alternate = UARTX_TX_AF;
HW_GPIO_Init(GPIOA, GPIO_PIN_9/*this point change*/, &GPIO_InitStruct);
/* UART RX GPIO pin configuration */
GPIO_InitStruct.Alternate = UARTX_RX_AF;
HW_GPIO_Init(GPIOA, GPIO_PIN_10/*this point change*/, &GPIO_InitStruct);
/*##-3- Configure the NVIC for UART ########################################*/
/* NVIC for UART */
NVIC_SetPriority(UARTX_IRQn, 0);
NVIC_EnableIRQ(UARTX_IRQn);
/* enable RXNE */
LL_LPUART_EnableIT_RXNE(UARTX);
}
void vcom_IoDeInit(void)
{
GPIO_InitTypeDef GPIO_InitStructure = {0};
GPIO_InitStructure.Mode = GPIO_MODE_INPUT;
GPIO_InitStructure.Pull = GPIO_NOPULL;
HW_GPIO_Init(GPIOA, GPIO_PIN_9/*this point change*/, &GPIO_InitStructure);
HW_GPIO_Init(GPIOA, GPIO_PIN_10/*this point change*/, &GPIO_InitStructure);
}