Associate II
October 29, 2019
Solved
Dropouts in ADC capture on STM32H743
- October 29, 2019
- 22 replies
- 6689 views
If I connect a constant rising signal at the ADC input, I observe significant fluctuations at certain ADC values. These fluctuations always appear at the same ADC values. The affected values have the following format XX500, e.g. 18500, 19500, 20500 etc.
I was also able to reproduce this behavior with the NUCLEO-H743ZI and the example projects (ADC_DMA_Transfer and ADC_RegularConversion_Polling) from the current cube firmware V1.5.0. The graphic in the appendix shows a recorded ADC values, which shows the problem.
Can someone help me to solve the problem?