Skip to main content
NGama
Associate II
October 28, 2019
Solved

Border Router with Thread Network

  • October 28, 2019
  • 3 replies
  • 1203 views

Are there any application notes or references about a border router used with a Thread network because I hadn't found any.

This topic has been closed for replies.
Best answer by Remi QUINTIN

I assume that as long as the new board is supporting the Thread protocol on one side and an internet connection on the other side using either a wired connection or a separate Wi-Fi module, it should be OK.

3 replies

Remi QUINTIN
ST Technical Moderator
October 29, 2019

​The border router use case is not supported by the Thread stack provided for the STM32WB.

The Thread + Ethernet or wifi connectivity is missing to fulfill this feature.

NGama
NGamaAuthor
Associate II
October 30, 2019

Is there any way to connect a raspberry pi to the network and use that as the border router?

Remi QUINTIN
Remi QUINTINBest answer
ST Technical Moderator
October 30, 2019

I assume that as long as the new board is supporting the Thread protocol on one side and an internet connection on the other side using either a wired connection or a separate Wi-Fi module, it should be OK.