Skip to main content
Vvk.755
Associate II
October 28, 2019
Question

Hi All, Does anybody used STUSB4500 A_B_SIDE signal for mux selecting TUSB542 IC. Regards, Vyshnav Krishnan

  • October 28, 2019
  • 2 replies
  • 764 views

..

    This topic has been closed for replies.

    2 replies

    Gregory Go.
    Senior III
    December 6, 2019

    Hello,

    The A_B_SIDE pin of STUSB4500 tells you the orientation of the USB-C cable.

    - If the A_B_SIDE pin is at level '1', it means the CC line (of the USB-C cable) is connected to CC1 pin.

    - If the A_B_SIDE pin is at level '0', it means the CC line (of the USB-C cable) is connected to CC2 pin.

    Thus you can know which pins are used for USB 3.x data transfer:

    - If CC1 is used, then the USB 3.x SuperSpeed signals are coming from TX1+/TX1- and RX1+/RX1- (i.e. the SuperSpeed pins closer to CC1 pin).

    - If CC2 is used, then the USB 3.x SuperSpeed signals are coming from TX2+/TX2- and RX2+/RX2-

    Best regards.

    Vvk.755
    Vvk.755Author
    Associate II
    December 27, 2019

    Hi Gregory,

    Thank you for your valuable response. In my design I have used A_B_SIDE of STUSB4500 to select TUSB542 USB 3.0 re-driver. But USB3.0 is not getting detected. The USB3.0 Device is detected as high speed device, than super speed device.

    Regards,

    Vyshnav Krishnan