Skip to main content
Singh.Harjit
Senior
October 27, 2019
Question

DS12288 - STM32G474xB Datasheet - Errors

  • October 27, 2019
  • 3 replies
  • 854 views
  1. Page 118, Table 38 has "1.78" in Peripheral column instead of TIM1.
  2. Page 115, fourth bullet says "... is given in Table 39. The power...". The table number should be 38.
This topic has been closed for replies.

3 replies

ST Technical Moderator
October 31, 2019

Hello @Singh.Harjit​ ,

I think the first error is fixed in the DS12288 Rev 2.

Can you please check this ?

Best Regards,

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
Singh.Harjit
Senior
October 31, 2019

Indeed it is! Thank you.

A couple minor items in Rev 2 - should I create a new thread since it is against Rev 2 and this thread has Rev 1 in the title?

  1. Section 2, page 13, half way down the page it says: twothree general-purpose 32-bit timers
  2. Section 3.6, page 19, Figure 2 shows SRAM1 on the I-bus and D-bus which doesn't match the description in section 3.5.

I was very glad to see the information in Tables 74 - 76.

ST Technical Moderator
November 11, 2019

Hello @Singh.Harjit​ ,

Thank you for pointing out the errors.

We will correct these in the next release of STM32G474 Datasheet.

Best Regards,

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks