Skip to main content
mattb3.14159
Associate II
October 24, 2019
Question

30 second timeout whilst programming external device with custom external loader in STM32CubeProgrammer

  • October 24, 2019
  • 2 replies
  • 854 views

I have written an external loader for a device connected to my STM32F103 and I have debugged it and it works for the most part. Init(), Erase(), SectorErase(), Read() and Write() are all working ok, except when trying to program a large file. My external device is fairly slow to program (a couple of minutes) but it looks like STM32CubeProgrammer is interrupting the programming after about 30 seconds. Is there some sort of timeout in STM32CubeProgrammer?

I have a debug version of my project setup (standalone) and call Init(), then Write() with the same data and it takes a couple of minutes but it gets there. I have replicated the stack space and location (I got that from the STM32CubeProgrammer log) of 1024 bytes and located right above the code and data in RAM.

Any ideas if there is a timeout in STM32CubeProgrammer on the write cycle?

This topic has been closed for replies.

2 replies

mattb3.14159
Associate II
October 24, 2019

Forgot to put the log in

mattb3.14159
Associate II
October 25, 2019

I was just trolling through the log and it a sector erase is done, and then the file is broken up into chunks.

From my elf file:

 449: 20000e85  110 FUNC  GLOBAL DEFAULT  4 Init

  450: 20000ef3  32 FUNC  GLOBAL DEFAULT  4 Read

  451: 20000f13  32 FUNC  GLOBAL DEFAULT  4 Write

  452: 20000f33  26 FUNC  GLOBAL DEFAULT  4 MassErase

  453: 20000f4d  30 FUNC  GLOBAL DEFAULT  4 SectorErase

The first call of the Write() function from the log is:

Write( 0, 0xA600, 0x20030C0 ); // int Write( uint32_t Address, uint32_t Size, uint8_t * buffer )

The next call is exactly the same, the buffer address has not been incremented:

Write( 0, 0xA600, 0x20030C0 );

which is just writing over the previously written data in my external device.