Debugging an imported project from Cube MX into workbench STM32
- October 24, 2019
- 2 replies
- 2120 views
Hallo ,
I am trying to debug an imported project from CubeMx, which is just the configuration of the STM32MP!57C-DK2 board, I built the solution in the system workbench and then connected to the board. on the Console I cannot see any IP Address for the board, so i used ifconfig, and i entered the eth0 ip address in the debug configuration, when i debug the solution, i end up with this error message(attached).
I attached my debug configuration as well. I also tried port 3333 which got the same problem
I tried to debug just the OPENAMP_TTY example, it cannot be compiled (Photo- OpenAMP)
I wonder what is wrong?. Your help is very much appreciated
Note; Regarding the OpenAMP problem, I saw the answered question, i followed the answer but the problem still exists. Maybe there should be some sort of special ocd or gdb config?. I am not sure as am totally new to that board
Thanks in Advance