How much can I overclock the STM32F303xx MCUs when powered by 3.3v and running at room temperature?
I'm using the STM32F303xx MCU in an application with a 24.576MHz crystal. The MCU is powered from 3.3v. I am currently clocking the processor at 3x 24.576MHZ, or just slightly under 74MHz. I realize this is above the rated maximum processor clock of 72MHz but I thought it will work anyway, especially since the MCU is rated down to 2.0v and I am using 3.3v and only using it at ambient room temperature.
What I'm wondering is, can I reliably increase the processor clock to 4x 24.576MHz = 98.304MHz under these conditions? I tried it and it seems to work but I don't want to run into any unexpected reliability issues down the road. In my understanding increasing the supply voltage should definitely increase the maximum operating frequency but there is no such information in the datasheet.
I would appreciate any more helpful information you can provide.
Thanks!
-Brian