Skip to main content
MikeDB
Senior II
October 20, 2019
Question

H7 series peripheral performance in VOS2 and 3

  • October 20, 2019
  • 7 replies
  • 1333 views

The datasheets for the interface characteristics of each peripheral state "VOS level set to VOS1" which is the 400MHz option. But no information is given on if any of the peripherals derate if you use the slower speed and power VOS options. Would especially be interested in whether the max speed of the SPI1-3 degrade from 100MHz. I'm suspecting they might as SPI4-6 are in a different power area and only run at 50MHz.

This topic has been closed for replies.

7 replies

TDK
October 20, 2019

Look at "Table 55. Kernel clock distribution overview".

The SPI data rate can be half of the kernel clock rate (with a prescaler of 2), subject to the maximums in the table.

So SPI1,2,3 can be 100/100/75/50 Mbit/s max at VOS0/VOS1/VOS2/VOS3.

And SPI4,5,6 can be 62.5/50/37.5/25 Mbit/s max.

(Presumably the second "VOS2" column is a typo and should read "VOS3".)

"If you feel a post has answered your question, please click ""Accept as Solution""."
MikeDB
MikeDBAuthor
Senior II
October 20, 2019

Can you give me a link to the document you are referencing. In the one I am using Table 55 is about ESD and it sounds like the one you have is what I need.

Tesla DeLorean
Guru
October 20, 2019
Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
TDK
October 20, 2019

RM0433

"If you feel a post has answered your question, please click ""Accept as Solution""."
MikeDB
MikeDBAuthor
Senior II
October 20, 2019

Hmm - RM0433 says max 100Mbps for VO1 as you say, but the datasheet says 133 MHz. I'll assume the slower of the two.

TDK
October 20, 2019
Seems safe. There are a few different H7 lines with different datasheets and reference manuals. It’s possible it varies. You didn't mention which chip you’re using so I just guessed
"If you feel a post has answered your question, please click ""Accept as Solution""."