Skip to main content
Pavel A.
October 16, 2019
Solved

Debug interface of STM32H7 question

  • October 16, 2019
  • 3 replies
  • 1648 views

Dear experts,

I'm new to M7 (and H7) so pardon me for a stupid question.

Created a new .ioc file in CubeMX 5.3.0 for STM32H753 EVAL2 board.

There I can select debug interface as JTAG 5 pins or Serial wire (at least).

From the Cube report file, in Serial Wire mode it uses 2 pins:

PA14 SWCLK

PA13 SWDIO

Where is SWO ? It should be PB3, but the report file does not mention it.

In JTAG 5 pins mode it uses

PA14, PA15, PA13, PB3, PB4.

Now, in a .ioc file made by my hardware engineer, for a custom board with same MCU,

the debug mode is JTAG 5 pins.

But I cannot change it to Serial wire or even to Disabled.

Any reason, why?

None of these 5 pins are hmm... pinned.

Serial mode uses two (or three?) of JTAG 5 pins, so it should be possible to reuse them?

Is the JTAG config locked by some other component or mode selection?

Or can it be a "feature" of the Cube ?

We both have Cube 5.3.0 on Linux, Ubuntu,

Thanks in advance

Pavel A.

This topic has been closed for replies.
Best answer by Tesla DeLorean

Boundary scan needs a lot of detail to execute properly, I worked with guys that build JTAG tools, schematic/net-list post-processing tools, and such.

You'd need JTAG to talk to multiple STM32 in a chain, or chained with FPGA/CPLD.

We've used it in the past to check boards, pin-to-pin continuity, etc.

3 replies

Tesla DeLorean
Guru
October 17, 2019

Well TDO/SWO on PB3 does work, the plumbing is more complicated as you need to configure which MCU connects up.

You're persistent in the face of much brokenness. I don't think much of CubeMX gets tested in real-world situations, and definitely not with any rigor.

Full JTAG at least permits boundary scan, and you can chain in other components. Unless you're completely bereft of pins I would avoid committing them,

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Pavel A.
Pavel A.Author
October 17, 2019

Clive,

Do you recommend JTAG mode over SWD for H7?

I've used only SWD mode before with F4, F0 and various ST-LINKs

Is boundary scan useful for the STM32 at all?

Thank you.

-- pa

Tesla DeLorean
Tesla DeLoreanBest answer
Guru
October 17, 2019

Boundary scan needs a lot of detail to execute properly, I worked with guys that build JTAG tools, schematic/net-list post-processing tools, and such.

You'd need JTAG to talk to multiple STM32 in a chain, or chained with FPGA/CPLD.

We've used it in the past to check boards, pin-to-pin continuity, etc.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..