Skip to main content
Eleon BORLINI
ST Employee
October 11, 2019
Question

SensorTile.box #7: Expert mode application at work - the Free fall detection

  • October 11, 2019
  • 1 reply
  • 1067 views

Now it's time to create your own app in Expert View (Mode 2). This mode allows the creation of custom app by allowing the user to select one or more input source available. These functions can be configured and optimized for each use case.

In addition, the ST BLE Sensor App also allows you to define specific conditions and actions based on the different functions implemented within the algorithm. For example, when implementing a free-fall detection, the app can count the number of detected events

The mobile application will then plot and count the number of events detected and data logging can also be enabled in this mode for further data analysis.

0690X00000ApWzNQAV.png

And, finally, LED toggle upon the detection of that specific event 8)

    This topic has been closed for replies.

    1 reply

    Eleon BORLINI
    ST Employee
    October 11, 2019

    0690X00000ApX69QAF.png