Skip to main content
ramkumarkoppu
Associate III
October 9, 2019
Solved

Mismatch STM32H747I-DISCO board configuration in STM32CubeMX .

  • October 9, 2019
  • 10 replies
  • 2132 views

As per the section 5.2.3 of the STM32H747I-DISCO board user manual, the default configuration of the hardware is to use SMPS mode but the default mode generated by STM32CubeMX when you select STM32H747I-DISCO board is LDO. Because of this mismatch, the board is bricked.

ST should have used the same power supply configuration in both the hardware board and default CubeMX configuration.

This topic has been closed for replies.
Best answer by Khouloud ZEMMELI

​You're right @ramkumarkoppu​ this issue has been fixed and it will be available in the 5.4.0 CubeMX version.

0690X00000ApOqmQAF.png

Best regards,

Khouloud.

10 replies

Khouloud ZEMMELI
ST Employee
October 10, 2019

​Hello @ramkumarkoppu​ ,

Thanks for your feedback,

CubeMX gives you the choice to choose which supply source you like , so  you can change this parameter under RCC configuration .

Best regards,

Khouloud

ramkumarkoppu
Associate III
October 10, 2019

Hi @Khouloud ZEMMELI​ There is no option in CubeMX specifically for PWR_DIRECT_SMPS_SUPPLY.

Khouloud ZEMMELI
Khouloud ZEMMELIBest answer
ST Employee
October 10, 2019

​You're right @ramkumarkoppu​ this issue has been fixed and it will be available in the 5.4.0 CubeMX version.

0690X00000ApOqmQAF.png

Best regards,

Khouloud.

ramkumarkoppu
Associate III
October 10, 2019

And also Core Boot selection is grayed out. I can't see option in CubeMX to select CPU core. Is this something will be available in the next version?

Khouloud ZEMMELI
ST Employee
October 10, 2019

For RCC both cortexs are available ​.

ramkumarkoppu
Associate III
October 10, 2019

I mean, In the dual core micro controller STM32H747, In the CubeMX, we don't have option to enable just one core and disable the other. Is it something possible with the current version of CubeMX ?

Khouloud ZEMMELI
ST Employee
October 10, 2019

​Ah, no this's not possible for the moment.

ramkumarkoppu
Associate III
October 10, 2019

Can you please add this option in the next version. It will be handy.

Khouloud ZEMMELI
ST Employee
October 10, 2019

​I'll be share your request with the team .

This will be internally checked.

Best Regards,

Khouloud.

ramkumarkoppu
Associate III
October 10, 2019

Cheers @Khouloud ZEMMELI​