Skip to main content
MMatu
Associate II
October 8, 2019
Solved

NUCLEO-H745 + ST-Link Utility = Can not connect to target

  • October 8, 2019
  • 5 replies
  • 2527 views

Dear STM Community

I am facing a problem with flashing/erasing STM32H745 microcontroller using STM32-ST Link Utility. Everytime I try to perform any operation I receive popular "Can not connect to target! If you're trying to connect to a low frequency application, please select a lower SWD Frequency...."

So I did that. I went to Target -> Settings. ST-LINK, Serial Number and Firmware of ST-LINK V3 were recognized correctly. I was even able to upgrade the firmware. But setting Mode to Normal or Connect Under Reset or lowering the frequency of SWD is not helping me with connect to, flash or erase the chip. Is there anything I can do to fix this?

This topic has been closed for replies.

5 replies

Tesla DeLorean
Tesla DeLoreanBest answer
Guru
October 8, 2019
Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
MMatu
MMatuAuthor
Associate II
October 8, 2019

Thank you Clive for your quick reply. I don't have any goldpins soldered to the board yet so I need to do that first before I check this BOOT0 method but I will get back with some updates ASAP.

Tesla DeLorean
Guru
October 8, 2019

ST really needs to jumper BOOT0 on all the dual core boards, most everyone is going to brick the device at some point during debug/development.

Metal tweezers or micro-grippers also work. The BT0 and VDD/GND are conveniently located.

I'd generally recommend a 500ms idle loop in main() prior to calling SystemClock_Config().

Not sure the ST-LINK/V3 supports a connect-under-reset mode currently.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
CGauk
Visitor II
June 22, 2020

I used the spring of a bent paper clip to keep a short between the 3V3_VDD and BT0 (BOOT0) holes to cause the Boot into the System ROM. This allows a connect with ST-LINK/V3 and then Erase the Chip to recover a bricked Nucleo-STM32H745. Remove the short after erasing.