Skip to main content
Central SUPPORT
Senior
October 4, 2019
Solved

Calculate stepss for PowerSTEP01 (and L6480)

  • October 4, 2019
  • 4 replies
  • 3155 views

Hi, I am currently implementing software/firmware for the PowerSTEP01 chip and discovered a inconsistency in data sheet https://www.st.com/resource/en/datasheet/powerstep01.pdf. For parameter INT_SPEED (section 11.1.11 in datasheet) the equation does correspond to the stated limits.

It says:

0690X000009k1YHQAY.jpg

i.e. steps/s = INT_SPEED × (2^−18) ÷ (250×10^−9)

  • For smallest possible INT_SPEED=1 you get the minimum value:

steps/s = 1 × (2^−18) ÷ (250×10^−9) = 15.25

  • For largest possible 14 bit value you get the maximum value:

step/s = (2^(14+1)−1) × (2^−18) ÷ (250×10^−9) = 499984.74

But according to datasheet equation results should be in range 0 < steps/s < 976.5.

So what is correct?

NOTE: This question and answer originated from a customer support case which was handled by us. We regularly review support cases and add any helpful ones here for all to benefit from.

              

This topic has been closed for replies.
Best answer by Central SUPPORT

You are right, thank you for raising this issue. In fact, there is a typo in datasheet. The correct formula is:

0690X000009k1ZKQAY.jpg

i.e. steps/s = INT_SPEED × (2^−26) ÷ (250×10^−9)

Same mistake applies also to L6480 datasheet :persevering_face: , but at least L6470 datasheet is correct :) . Control logic is the same for all 3 devices.

Mistake in datasheet will be corrected asap. Sorry for the inconvenience.

4 replies

Central SUPPORT
Central SUPPORTAuthorBest answer
Senior
October 4, 2019

You are right, thank you for raising this issue. In fact, there is a typo in datasheet. The correct formula is:

0690X000009k1ZKQAY.jpg

i.e. steps/s = INT_SPEED × (2^−26) ÷ (250×10^−9)

Same mistake applies also to L6480 datasheet :persevering_face: , but at least L6470 datasheet is correct :) . Control logic is the same for all 3 devices.

Mistake in datasheet will be corrected asap. Sorry for the inconvenience.

MHall.4
Associate
February 15, 2022

I have just downloaded the 'latest' datasheet and this change has not been implemented

Explorer
September 23, 2024

I second MHall.4,

ST, we'd like more clarity on this. A datasheet revision would be very nice.

Cristiana SCARAMEL
ST Employee
November 4, 2024

Hello @MHall.4 & @jagor34 

finally you can download the last datasheet revision of powerSTEP01;)

"If you feel a post has answered your question, please click ""Accept as Solution"""