Skip to main content
KR51K
Associate III
October 2, 2019
Question

Stuck in UART_WaitOnFlagUntilTimeout

  • October 2, 2019
  • 0 replies
  • 788 views

Hi,

I'm trying to transmit/receive data by uart. I have a state machine that is processing incoming bytes periodically, so I use a ringbuffer and write every received byte into this buffer.

void HAL_UART_RxCpltCallback(UART_HandleTypeDef *huart)

{

  if (huart == &uart3)

  {

   fFifoIn( &RX_BUFFER, RX_UART4_Buffer[0]);

   HAL_UART_Receive_IT( &huart4, RX_UART4_Buffer, RX_BUFFER_SIZE);

  }

}

I had to call HAL_UART_Receive_IT afterwards otherwise receiving stopped after one byte (found here: https://riptutorial.com/de/stm32/example/29940/echoanwendung---hal-bibliothek)

Transmitting of data is done by HAL_UART_Transmit.

Normally I'm requesting data from the communication part that is send periodically after requesting them once. My problem is, that sometimes the communication does not start. With debugging I found, that it stucks in the UART_WaitOnFlagUntilTimeout, but I don't know why and how to handle this. Any ideas?

Thanks and best regards

Christoph

This topic has been closed for replies.