Skip to main content
NW27
Associate II
October 2, 2019
Question

Getting started with the P-L496G-CELL02

  • October 2, 2019
  • 1 reply
  • 534 views

Hi,

I have downloaded and installed the STM32CubeIDE and have used it to do a blinky LED on a NUCLEO-L476RG, so basically have a bit of an understanding of the IDE and coding/compiling & burning.

However, I'm lost as to how to proceed in getting my P-L496G-CELL02 board to connect to Azure??

I have connected via TeraTerm and registered the board at http://www.stm32-c2c.com

( I have installed a Telstra micro SIM for the CAT-M1 Network)

What do I need to download for the compiler?

Thanks,

Neil.

This topic has been closed for replies.

1 reply

Guillaume K
ST Employee
October 8, 2019