ESC based on STEVAL-SPIN3201 and STSPIN32F0
Hello,
I`m currently thinking of creating stripped down version of STEVAL-SPIN3201. I have a few questions before I can start with this project:
Why is there STM32F103CBT6 MCU on the STEVAL-SPIN3201 evaluation board? I can`really see much purpose for this chip.
Is it possible to use PWM signal (as standard RC servo signals, a 1-2ms. wide pulse every 20ms) as speed control input signal (throttle) to STSPIN32F0 chip?
Basically I would like to build ESC based on STEVAL-SPIN3201, leave out STM32F103CBT6 MCU part and control the speed of the motor with sending PWM signal from my drone`s controller board to STSPIN32F0. Is that possible?
I can see that STEVAL-ESC002V1 requires PWM input for controlling the speed of the motor. So this should be possible with STEVAL-SPIN3201 also.
How is the actual speed controlling signal part meant to be implemented on STEVAL-SPIN3201? Via USART?
Thank you!