Question
ST-LINK_gdbserver and failing gdb "compare-section" command
Starting ST-LINK_gdbserver with -the -s option, flash upload show success. However the "compare-section" command show mismatch"
(gdb) compare-section
Section .text, range 0x8000000 -- 0x8003420: MIS-MATCHED!
Section .data, range 0x8003420 -- 0x80035bc: MIS-MATCHED!
warning: One or more sections of the target image does not match
the loaded file
Using another gdb-server (bl*ckm*g*i_pcstlinkv2) compares fine in the same setup even without another upload.