Skip to main content
michal_ca
Associate II
September 26, 2019
Question

STM32H743 Parallel synchronous transmission with DMA and GPIO

  • September 26, 2019
  • 4 replies
  • 1943 views

Hi all,

I have problem to get work stm32h743 as parallel synchronous transmission with DMA and 16bits GPIO and timer as clok. I need something like in Application note AN4666 but for H7xx.

I'm using GPIO port E what is on AHB4 and it si D3 domain and Timer 1 chanel 1 pwm output as clok. TIM1 is on APB2

pwm is running but i don't get any data from Port E

here is some documentation what i going through but no success .

en.DM00306681, en.DM00387108, RM0433

I'm using SW4STM32 and HAL lib.

Any advice ?

Thank you

In main()

if(enable == 1){
 
	SCB_CleanInvalidateDCache();
	HAL_DMA_Abort(htim1.hdma[TIM_DMA_ID_CC1]);
	HAL_DMA_DeInit(htim1.hdma[TIM_DMA_ID_CC1]);
 
	MX_DMA_Init();
	MX_TIM1_Init();
 
 
	/* USER CODE BEGIN 2 */
	//HAL_TIM_PWM_Start(&htim2, TIM_CHANNEL_1);
	htim1.hdma[TIM_DMA_ID_CC1]->XferCpltCallback = TransferComplete;
	htim1.hdma[TIM_DMA_ID_CC1]->XferErrorCallback = TransferError;
 
	if (HAL_DMA_Start_IT(htim1.hdma[TIM_DMA_ID_CC1], (uint32_t)&asrc_buffer, (uint32_t)&(GPIOE->ODR), FULL_FRAME_SIZE) != HAL_OK)
	{
	 /* Transfer Error */
	 Error_Handler();
	}
 
	__HAL_DMA_DISABLE_IT(htim1.hdma[TIM_DMA_ID_CC1], DMA_IT_HT);
	__HAL_TIM_ENABLE_DMA(&htim1, TIM_DMA_CC1);
 
	/*Start TIM PWM channel 1 */
	if (HAL_TIM_PWM_Start(&htim1, TIM_CHANNEL_1) != HAL_OK)
	{
		//PWM Generation Error
		Error_Handler();
	}
	enable = 0;
	HAL_Delay(500);
 
}
 

init

void HAL_TIM_PWM_MspInit(TIM_HandleTypeDef* htim_pwm)
{
 if(htim_pwm->Instance==TIM1)
 {
 /* USER CODE BEGIN TIM1_MspInit 0 */
 /* USER CODE END TIM1_MspInit 0 */
 /* Peripheral clock enable */
 __HAL_RCC_TIM1_CLK_ENABLE();
 
 /* TIM1 DMA Init */
 /* TIM1_CH1 Init */
 hdma_tim1_ch1.Instance = DMA2_Stream6;
 hdma_tim1_ch1.Init.Request = DMA_REQUEST_TIM1_CH1;
 hdma_tim1_ch1.Init.Direction = DMA_MEMORY_TO_PERIPH;
 hdma_tim1_ch1.Init.PeriphInc = DMA_PINC_DISABLE;
 hdma_tim1_ch1.Init.MemInc = DMA_MINC_ENABLE;
 hdma_tim1_ch1.Init.PeriphDataAlignment = DMA_PDATAALIGN_BYTE;
 hdma_tim1_ch1.Init.MemDataAlignment = DMA_MDATAALIGN_BYTE;
 hdma_tim1_ch1.Init.Mode = DMA_NORMAL;
 hdma_tim1_ch1.Init.Priority = DMA_PRIORITY_HIGH;
 hdma_tim1_ch1.Init.FIFOMode = DMA_FIFOMODE_DISABLE;
 //hdma_tim1_ch1.Init.FIFOThreshold = DMA_FIFO_THRESHOLD_1QUARTERFULL;
 hdma_tim1_ch1.Init.MemBurst = DMA_MBURST_SINGLE;
 hdma_tim1_ch1.Init.PeriphBurst = DMA_PBURST_SINGLE;
 if (HAL_DMA_Init(&hdma_tim1_ch1) != HAL_OK)
 {
 Error_Handler();
 }
 __HAL_LINKDMA(htim_pwm,hdma[TIM_DMA_ID_CC1],hdma_tim1_ch1);
 /* USER CODE BEGIN TIM1_MspInit 1 */
 
 /* USER CODE END TIM1_MspInit 1 */
 }
}

init TIM1 PWM is running at 1.3MHz

static void MX_TIM1_Init(void)
{
 
 /* USER CODE BEGIN TIM1_Init 0 */
 
 /* USER CODE END TIM1_Init 0 */
 
 TIM_OC_InitTypeDef sConfigOC = {0};
 
 /* USER CODE BEGIN TIM1_Init 1 */
 
 /* USER CODE END TIM1_Init 1 */
 htim1.Instance = TIM1;
 htim1.Init.Prescaler = 0;
 htim1.Init.CounterMode = TIM_COUNTERMODE_UP;
 htim1.Init.Period = 0xAA;
 htim1.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;
 htim1.Init.RepetitionCounter = 0;
 htim1.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_DISABLE;
 if (HAL_TIM_PWM_Init(&htim1) != HAL_OK)
 {
 Error_Handler();
 }
 sConfigOC.OCMode = TIM_OCMODE_PWM1;
 sConfigOC.Pulse = 0x55;
 sConfigOC.OCPolarity = TIM_OCPOLARITY_HIGH;
 sConfigOC.OCNPolarity = TIM_OCNPOLARITY_HIGH;
 sConfigOC.OCFastMode = TIM_OCFAST_ENABLE;
 sConfigOC.OCIdleState = TIM_OCIDLESTATE_RESET;
 sConfigOC.OCNIdleState = TIM_OCNIDLESTATE_RESET;
 if (HAL_TIM_PWM_ConfigChannel(&htim1, &sConfigOC, TIM_CHANNEL_1) != HAL_OK)
 {
 Error_Handler();
 }
 
 /* USER CODE BEGIN TIM1_Init 2 */
 
 /* USER CODE END TIM1_Init 2 */
 HAL_TIM_MspPostInit(&htim1);
 
}
static void MX_DMA_Init(void) 
{
 
 /* DMA controller clock enable */
 __HAL_RCC_DMA2_CLK_ENABLE();
 
 /* DMA interrupt init */
 /* DMA2_Stream6_IRQn interrupt configuration */
 HAL_NVIC_SetPriority(DMA2_Stream6_IRQn, 0, 0);
 HAL_NVIC_EnableIRQ(DMA2_Stream6_IRQn);
 
}

This topic has been closed for replies.

4 replies

waclawek.jan
Super User
September 26, 2019

Read out and check content of relevant TIM (_DIER), DMAMUX and DMA registers (and peripahs also the GPIOE registers).

Is the source memory DMA-ble (as per caching status)?

JW

michal_ca
michal_caAuthor
Associate II
October 3, 2019

Hi all,

I make it work with BDMA and LPTIM2 and SRAM4, but here is 50ns offset between Clock (LPTIM2 PWM) and 16bit gpio.

As I mentioned before I need parallel synchronous transmission so I would like to eliminate 50ns offset between clock and data.

I trying to make synchronisation at falling edge of CLK. And my goal is reach 16MHz.

It is even possible with STM32H7 ?

Thank you

0690X000009jzrbQAA.jpg3

0690X000009k06MQAQ.jpg

Regards

mv

DBurr
Senior
October 17, 2019

I'd like to attempt the same thing with the STM32F746 except using an 8 bit parallel interface, could you post your source code?

Thanks,

Doug Burrell

flyer31
Senior
August 30, 2020

See my solution how to do this with BDMA or DMA:

See my STM32H7 forum post "Parallel transmission using GPIO and DMA (like AN4666)"