STM32F205 uses TIM_DMA_Update event of timer 8 to trigger DMA2 circularly. In fact, DMA only executes once?
- 6 replies
- 1985 views
STM32F205 uses the TIM_DMA_Update event loop of timer 8 to trigger DMA2 transport, which moves 5 data from test_data to dest_arr at a time.
Using DMA2_Stream1_Channel7, start these two functions in the main program, configure DMA and TIM8, and then observe that the value of test_data changes to 0x06030444.
When test_data is cleared after a period of delay, the timer can enter the interrupt normally, but DMA no longer works. Test_data is always zero, and I don't know what the problem is.
Please help me to analyze it.
unsigned int dest_arr;
unsigned int test_data[5] = {0x06030440,0x06030441,0x06030442,0x06030443,0x06030444};
/*DMA configuration*/
void DMA_Auto_Config(void)
{
DMA_InitTypeDef DMA_InitStructure;
RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_DMA2,ENABLE);
DMA_DeInit(DMA2_Stream1);
while (DMA_GetCmdStatus(DMA2_Stream1) ! = DISABLE){} // wait DMA2_Stream1 disable
DMA_InitStructure.DMA_Channel = DMA_Channel_7; // select DMA_Channel_7
DMA_InitStructure.DMA_PeripheralBaseAddr = (uint32_t)(test_data); // source address
DMA_InitStructure.DMA_Memory0BaseAddr = (uint32_t)(&dest_arr); // Destination address
DMA_InitStructure.DMA_DIR = DMA_DIR_MemoryToMemory; // MemoryToMemory
DMA_InitStructure.DMA_BufferSize = 5;
DMA_InitStructure.DMA_PeripheralInc = DMA_PeripheralInc_Enable;
DMA_InitStructure.DMA_MemoryInc = DMA_MemoryInc_Disable;
DMA_InitStructure.DMA_PeripheralDataSize = DMA_PeripheralDataSize_Word;
DMA_InitStructure.DMA_MemoryDataSize = DMA_MemoryDataSize_Word;
DMA_InitStructure.DMA_Mode = DMA_Mode_Normal;
DMA_InitStructure.DMA_Priority = DMA_Priority_High;
DMA_InitStructure.DMA_FIFOMode = DMA_FIFOMode_Disable;
DMA_InitStructure.DMA_FIFOThreshold = DMA_FIFOThreshold_Full;
DMA_InitStructure.DMA_MemoryBurst = DMA_MemoryBurst_Single;
DMA_InitStructure.DMA_PeripheralBurst = DMA_PeripheralBurst_Single;
DMA_Init(DMA2_Stream1, &DMA_InitStructure);
DMA_Cmd(DMA2_Stream1, ENABLE);
}
/*timer8 configuration*/
void timer8_init(void)
{
GPIO_InitTypeDef GPIO_InitStructure;
TIM_TimeBaseInitTypeDef TIM_TimeBaseStructure;
TIM_OCInitTypeDef TIM_OCInitStructure;
NVIC_InitTypeDef NVIC_InitStructure;
RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOC, ENABLE);
RCC_APB2PeriphClockCmd(RCC_APB2Periph_TIM8, ENABLE);
TIM_TimeBaseStructure.TIM_Period = 100-1;
TIM_TimeBaseStructure.TIM_Prescaler = 60000-1;
TIM_TimeBaseStructure.TIM_ClockDivision = TIM_CKD_DIV1;
TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up;
TIM_TimeBaseInit(TIM8, &TIM_TimeBaseStructure);
NVIC_InitStructure.NVIC_IRQChannel = TIM8_UP_TIM13_IRQn;
NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0;
NVIC_InitStructure.NVIC_IRQChannelSubPriority = 2;
NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;
NVIC_Init(&NVIC_InitStructure);
TIM_ClearFlag(TIM8,TIM_FLAG_Update);
TIM_ITConfig(TIM8, TIM_IT_Update, ENABLE); // Enable TIM8 IRQ
TIM8->CR2 |= TIM_CR2_CCDS;
TIM_DMACmd(TIM8,TIM_DMA_Update,ENABLE);
TIM_Cmd(TIM8,ENABLE);
}
/*Main*/
int main(void)
{
uart5_init();
timer8_init();
DMA_Auto_Config();
delay_ms(100);
test_arr = 0;
while(1)
{
delay_ms(100);
printf("dest_arr = 0x%x\n",dest_arr);
}
return 0;
}
/*TIM8 irq*/
void TIM8_UP_TIM13_IRQHandler(void)
{
if(TIM_GetITStatus(TIM8,TIM_IT_Update)==SET)
{
TIM_Cmd(TIM8, DISABLE);
TIM_ClearITPendingBit(TIM8,TIM_IT_Update); // ClearITPendingBit
printf("TIMER_8 IRQ IRQIRQIRQIRQIRQIRQIRQIRQIRQIRQIRQIRQ!\n");
delay_ms(100);
TIM_Cmd(TIM8, ENABLE);
}
}
Output:(Dest_arr is always 0)
dest_arr = 0x0
TIMER_8 IRQ IRQIRQIRQIRQIRQIRQIRQIRQIRQIRQIRQIRQ!
TIMER_8 IRQ IRQIRQIRQIRQIRQIRQIRQIRQIRQIRQIRQIRQ!
TIMER_8 IRQ IRQIRQIRQIRQIRQIRQIRQIRQIRQIRQIRQIRQ!
dest_arr= 0x0
TIMER_8 IRQ IRQIRQIRQIRQIRQIRQIRQIRQIRQIRQIRQIRQ!