Skip to main content
Hungchul.Shin
Associate
September 25, 2019
Solved

How to be able to use the A7 cores without Linux ?

  • September 25, 2019
  • 1 reply
  • 759 views

Can I develop on IAR or Keil without Linux?

This topic has been closed for replies.
Best answer by Olivier GALLIEN

Hi @Hungchul.Shin​ 

IAR and KEIL support the STM32MP1 for the programming of the M4 core (coprocessor) , not the A7.

A7 bare metal is not a solution supported by ST. Some customers and third parties are working in this topic.

Be aware that if a peripheral driver is not available in CubeMP1 for M4 (which can be usually ported to A7), it is up to you to manage the SW.

This is the case for all peripherals which are different to support extended features of STM32MP1 family (e.g. ETH, GIC, BSEC, FMC, GPU, USBH, USBPHYC, DDRCTRL, DDRPHYC, etc..).

Olivier

1 reply

Olivier GALLIEN
Olivier GALLIENBest answer
ST Technical Moderator
October 1, 2019

Hi @Hungchul.Shin​ 

IAR and KEIL support the STM32MP1 for the programming of the M4 core (coprocessor) , not the A7.

A7 bare metal is not a solution supported by ST. Some customers and third parties are working in this topic.

Be aware that if a peripheral driver is not available in CubeMP1 for M4 (which can be usually ported to A7), it is up to you to manage the SW.

This is the case for all peripherals which are different to support extended features of STM32MP1 family (e.g. ETH, GIC, BSEC, FMC, GPU, USBH, USBPHYC, DDRCTRL, DDRPHYC, etc..).

Olivier

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.