Skip to main content
HLI.16
Associate
September 25, 2019
Question

Question on setting for NRG-1 and NRG-2

  • September 25, 2019
  • 4 replies
  • 696 views

I am using NRG-1 for my product development but I have only NRG-2 kit on hand. I am using NRG-2 project to develop my SW for using DK kit but I found there are 250kHz frequency offset when the software is applied to my HW for using NRG-1 inside. Is there any setting to be difference in NRG-1 and NRG-2 in latest 3.1.0 SDK apart from the high clock setting from 16M to 32M?

    This topic has been closed for replies.

    4 replies

    alok
    Visitor II
    September 29, 2019

    Generally, there shall be no difference in using BluNRG1 or BlueNRG-2. Did you review the tolerance of the XTAL of 16MHz ?

    Winfred LU
    ST Employee
    October 2, 2019

    Do you mean seeing 250kHz offset for some single tone?

    It would be expected behavior.

    For stack v2.x, a new parameter, offset, was introduce for ACI_HAL_TONE_START() API for user to start a tone at channel center frequencies without offsets.

    Please set the offset to 0.

    HLI.16
    HLI.16Author
    Associate
    October 8, 2019

    Yes. it is related to 250kHz offset problem. I used command of Radio_Start_tone() in our test code and this 250kHz will be still existed on it so it will give a difference behaviour for using DTM mode vs test code directly.

    Winfred LU
    ST Employee
    October 9, 2019

    Please get the DTM firmware from the latest SDK, STSW-BLUENRG1-DK v3.1.0 :

    https://www.st.com/en/embedded-software/stsw-bluenrg1-dk.html

    together with new GUI, STSW-BNRGUI v3.1.0 :

    https://www.st.com/content/st_com/en/products/embedded-software/wireless-connectivity-software/stsw-bnrgui.html