2019-09-23 5:44 AM
I am trying to communicate with an adc chip acting as a spi slave to my stm32f3 spi master. So far I am unable to make it work.
After attaching an oscillscope I found out that if i send only 8 bits of data to the slave , I get exactly 16 clock pulses on the SCLK of my master even though I have set the data size as 8.
My master config is
SPIx->CR1 |= SPI_CR1_SSI;
SPIx->CR1 |= SPI_CR1_SSM;
SPIx->CR1 |= SPI_CR1_BR_0 | SPI_CR1_BR_2;
SPIx->CR1 |= SPI_CR1_MSTR;
SPIx->CR1 |= SPI_CR1_CPOL;
SPIx->CR1 |= SPI_CR1_CPHA;
SPIx->CR1 |= SPI_CR2_DS_0 | SPI_CR2_DS_1 | SPI_CR2_DS_2;
SPIx->CR1 &= ~SPI_CR1_RXONLY;
SPIx->CR1 |= SPI_CR1_SPE;
SPIx->CR2 |= SPI_CR2_FRXTH;I write 8 bits simply as
while (!(SPIx->SR & SPI_SR_TXE));
SPIx->DR = 0x54;
while (!(SPIx->SR & SPI_SR_RXNE));
while (SPIx->SR & SPI_SR_BSY);I am NOT sending any dummy bytes from the master to read back from slave. Right now I just want to send 8 bits to slave and see 8 clock pulses.
Can someone tell me what might be going on here?
2019-09-23 7:21 AM
Ok so I found out that I had to access the DR in 8bit mode. That solved the extra clock cycles issue. Now I see another issue.
SCLK is not idling high even though I have set CPOL=1.
If I run a simple program from mbed and run on the hardware it is able to talk to the slave ADC just fine. The only difference between my implementation and the mbed program seems to be the clock.
Following is from my mbed program which is able to send command to adc and read back the reg. (sending 0x54=0b01010100 cmd)
Yellow is SPI clk, blue is MOSI
Pic below is from my own lowlevel SPI implementation
Yellow is SPI clk, blue is MOSI
The master clk in second pic is not idling high. Can this explain why I am unable to talk to the slave using my SPI config?
2019-09-23 7:51 AM
So basically in the second case I was sending the SPI msg from master immediately after enabling SPI. After adding artificial delay , now both mbed and my implementation CLK/MOSI signals look the same.
Still no answer from the slave spi (works with mbed program). Now I am at a total loss. any one got any ideas?
2019-09-23 8:20 AM
Do you use NSS signal with your ADC?
What is the ADC part number?
2019-09-23 8:48 AM
I have configured a GPIO pin as slave select and I do a manual SET/RESET on this pin. The ADC is Analog Devices 7913
2019-09-23 9:02 AM
I moved the HAL_GPIO_WritePin line just before my write_cmd and now it seems the slave chip is responding fine.
HAL_GPIO_WritePin(SPI_CS_GPIO_Port, SPI_CS_Pin, GPIO_PIN_RESET);
write_cmd(LOCK_KEY_READ);
recv_reg = write_cmd(0x00);Previously I was setting the pin low even before enabling the SPI module.
Does it matter how long before the CS was made low?(in my scenario CS low activates the slave)
Edit: In the ADC timing diagram I didn't find any constraint that CS has to be active just before transmission. Is this normal behaviour?
2019-09-23 10:22 AM
When a slave is not selected (CS high), usually its MOSI/MISO pins are high impedence (not listening to the bus).