Skip to main content
Bogdan Golab
Lead
September 19, 2019
Question

STM8 CubeMX v1.4.0 - only 2 timers shown for STM8S003F3

Hi,

I am pretty new to STM8 and CubeMX (have some experience in STM32).

----

I selected the STM8S003F3 and I can see only two timers - there should be TIM4 available but is not.

Another odd thing is that the TIM1&TIM2 are not available as long as no pins are free.

0690X00000AROC2QAP.jpg

The question for people using STM8 CubeMX: is this tool mature to use it? Or maybe I do not know how to use it?

    This topic has been closed for replies.

    3 replies

    Cristian Gyorgy
    Associate II
    September 20, 2019

    The TIM4 has no capture/compare channels, so no inputs/outputs to port pins. This is why it does not appear in the list.

    Bogdan Golab
    Lead
    September 20, 2019

    The STM32CubeMX shows all available resources. The STM8CubeMX works different way - only deals with pins....

    OK. Thanks.

    Bogdan Golab
    Lead
    September 20, 2019

    I assumed that both tools share the same philosophy. But STM8 version does not generate code skeleton - only allocates/shows available pins, I guess