Skip to main content
karthik.b
Associate II
September 19, 2019
Question

I need to program the ST8L101F3P6 with ST viual

  • September 19, 2019
  • 4 replies
  • 2618 views

hi,

       I am using ST8l101F3P6 microcontroller.

I have used ST Visual develop with Cosmic compiler.

I Programmed and compiled successfully.but I can not Program the controller with ST visual programmer..

when I try to program it asks to check the connections even though connections are made it correctly .

if I choose Tools > Programmer in STVD,IDE is automatically closed.

kindly share with solution.

    This topic has been closed for replies.

    4 replies

    KG?�l
    Associate II
    September 21, 2019

    I am using STVP with STLINKV2 to program STM8S003F3 and it is working. Connected ports are SWIM, NRST, VCC, GND. The only thing i couldn't solve , STVP not releasing NRST line after program. So every time i need to close STVP to run the chip. All these lines connected to STLINKV2 directly. I mean no pullups or pulldowns, no additional resistors etc.

    But i have another question for you. How did you get Cosmic compiler? Their download link not working.

    karthik.b
    karthik.bAuthor
    Associate II
    September 22, 2019
    cosmic compiler can be downloaded from ST website itself.
    Sent from vivo smartphone
    KG?�l
    Associate II
    September 23, 2019

    I couldn't find it. It is redirecting to cosmic web page which is not working anymore.

    KG?�l
    Associate II
    September 23, 2019

    I found the cosmic compiler and tried your case. One thing is same. If i try to run programmer from STVD , it is giving "Out of memory" error and closing. Sometime not even showing the error and just closing. I couldn't find solution for this.

    If i use programmer separately , it is working.