Skip to main content
odesc
Associate II
September 16, 2019
Solved

Increase EEPROM Erase/Write cycles capability for STM32L0

  • September 16, 2019
  • 10 replies
  • 4003 views

Hello all,

I am using the STM32L071KB in a project, and I have to write a 32 bit word in internal EEPROM each minute;

So is it worth changing the address of this 32 bit word after 100 000 cycles, in order to increase number of Erase/Write cycles ?

If the MCU erases the whole EEPROM at each Erase/Write cycle, that would not be worth. But I don't see this information in the user manual.

Thanks !

This topic has been closed for replies.
Best answer by waclawek.jan

The EEPROM erase granularity is word, i.e. 32 bits, in the 'L0 - and I believe did found that information in the RM. At least that's how it appears to the user; indeed, the true erase mechanism may involve internally buffering a larger page, erasing it, and writing it back. And mcu manufacturers - not only ST - for some strange reason very often don't advertise clearly the true mechanism even if it's a favourable one, i.e. if there's no such internal larger page.

If you are willing to spend one chip for the case, you can try it yourself; IMO a self-concocted test is definitive enough in this case. Of course, you can always try to ask ST - not here, this forum is visited by ST only casually - but through the web support form, or through your FAE, if you have one at hand.

JW

10 replies

Ozone
Principal
September 16, 2019

The word-wise erase/write capability and higher durability are normally features of EEPROM justifying its higher price in relation to FLASH.

I don't know the L071, but don't expect it to be different. I would double-check the datasheet.

First, the 100.000 number is usually guaranteed for the max. temperature, and roughly double for each 10C you go colder.

Second, consider a change in strategy. Like keeping data in RAM, and save only on power-off (or similar event).

odesc
odescAuthor
Associate II
September 16, 2019

Dear Ozone,

Thanks for your answer; in fact the op temperature can be relatively high, and we don't know when the MCU is powered OFF (so keeping data in RAM will not solve the problem).

That's why we would like to change the data address after 100 000 E/R cycles, but we don't know if it will solve the problem . ST doesn't decribe enough the EEPROM Erase/Write process.

Ozone
Principal
September 16, 2019

Starting a project involving EEPROM or FLASH erase/program begins with carefully reading the manuals:

The datasheet (DocID027101 Rev 3) says:

Flash program and data EEPROM are divided into two banks. This allows writing in one bank while running code or reading data from the other bank.

The reference manual (DocID025942 Rev 8) says:

0690X00000ARFPCQA5.png

Tesla DeLorean
Guru
September 16, 2019

You're either going to need to use an external EEPROM that meets your requirements, or create a more complex driver that manages cycle counts, and does wear-leveling. One of the most simple strategies being to journal writes across the memory, and then recover the last written values, rather than grinding data on a single spot.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
waclawek.jan
waclawek.janBest answer
Super User
September 16, 2019

The EEPROM erase granularity is word, i.e. 32 bits, in the 'L0 - and I believe did found that information in the RM. At least that's how it appears to the user; indeed, the true erase mechanism may involve internally buffering a larger page, erasing it, and writing it back. And mcu manufacturers - not only ST - for some strange reason very often don't advertise clearly the true mechanism even if it's a favourable one, i.e. if there's no such internal larger page.

If you are willing to spend one chip for the case, you can try it yourself; IMO a self-concocted test is definitive enough in this case. Of course, you can always try to ask ST - not here, this forum is visited by ST only casually - but through the web support form, or through your FAE, if you have one at hand.

JW

odesc
odescAuthor
Associate II
September 17, 2019

Hi JW,

Yes, this si exactly the problem; we don't know if erasing a 32 bit word erases in fact just the 32 bit word, or a whole page (buffered in RAM and writed back to Flash).

I have asked 2 days agao to ST support, but no answer yet...

odesc
odescAuthor
Associate II
September 18, 2019

Hi,

ST support just answered us :

the EEPROM in STM32L071 is organized by words (4 bytes) and erase operation erases only selected word. Thus 100k cycles is valid per each word separately.

And they confirm that we can write several millions of times the same data in EEPROM, if we increment the address every 100k cycles.

So very good news !

Olivier

waclawek.jan
Super User
September 18, 2019

Thanks for sharing the information.

ST, might consider adding this information clearly into the L0 DS/RM, or maybe better yet, writing an appnote (in black and white please). The EEPROM ought to be one of the selling points of the 'L0 line, but IMO the available materials fail to emphasize this, in clear and complete engineering terms, and this thread witnesses that too.

JW

@Imen DAHMEN​ , @Amel NASRI​ 

ST Technical Moderator
September 27, 2019

Hello @Community member​ ,

Good point. I raised the request for change in the coming reference manuals.

Best Regards,

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
waclawek.jan
Super User
September 27, 2019

Thanks.

JW