Skip to main content
DWang
Associate
September 15, 2019
Question

How to perform a factory reset for SensorTile?

  • September 15, 2019
  • 31 replies
  • 5427 views

Hi

Is there a way to perform a factory reset for SensorTile? For some reason, my laptop can't detect it anymore. Device manager said "This device cannot start. (Code 10). A device which does not exist was specified." I try to erase full chip flash memory and plan to load the original bootloader, but I also get error message in CubeProgrammer

"Error: Invalid port name: No DFU detEstablishing connection with the device failed"

 Pressing the root button doesn't seem to help. I first tried to press the button after connecting to a laptop, but it didn't help. I also tried to hold the root button and release it after connecting to the laptop, but it also didn't help.

May I know what I am missing?

Thanks,

Dennis

    This topic has been closed for replies.

    31 replies

    Eleon BORLINI
    ST Employee
    September 16, 2019

    Hi Dennis, it seems the os is not recognizing the stm32 device... a couple of HW question for my understanding: how are you using the SensorTile? I mean, is it plugged on the cradle expansion board or is soldered on the cradle? In this second case, is it connected to the battery (regardless the USB connection) and is the battery charged? Could you also check the soldering is ok? Regards

    DWang
    DWangAuthor
    Associate
    September 16, 2019

    Hi Eleon,

    Thanks for the quick reply and sorry for the confusion. I should clarify that I was using SensorTile.box. I didn't use the battery. I just give it another shot by pressing the root button before plug it into my laptop. It is able to enter DFU mode and flash the original bootloader. However, for some reason, I can't connect it through UART interface in STM32CubeProgrammer and Tera Term. Device Manager sees it as a USB drive instead of a COM port device. Would this be a driver issue? Or is the hardware is damaged?

    Eleon BORLINI
    ST Employee
    September 17, 2019

    Hi Dennis, I anyway suggest you to plug the battery during SensorTile.box operation. So help me to understand the issue: which default FW did you download on the SensorTile.box uC? Did you use the STBLE app to detect and download the last FW? ​If you want to use the USB to stream data, you can select "Stream to USB" from the app expert mode. Regards

    DWang
    DWangAuthor
    Associate
    November 19, 2019

    Hi Eleon,

    That would be awesome if it can be repaired!

    May I know what address I should ship to? Should I address any personnel on the package? And do I need to provide a return envelope?

    Thanks,

    Dennis

    Eleon BORLINI
    ST Employee
    November 21, 2019

    Hi Dennis, please check private messages. Regards

    DWang
    DWangAuthor
    Associate
    November 25, 2019

    Got it, thanks. Will email you privately. Thanks!