Skip to main content
VKALE
Associate II
September 12, 2019
Question

Did anyone tested audio playback on STM32746G-Discovery board, for any STM32F7 SDK version?

  • September 12, 2019
  • 0 replies
  • 523 views

Hi ST community,

Did anyone tested audio playback on STM32746G-Discovery board? May be one of the following use cases:

(1) Audio_playback_and_record which is available in Applications/Audio folder OR

(2) any simple use case just to play the audio PCM data, stored in an array?

I am having issues with both of the above and I opened a discussion thread for (1).

But before proceeding further, I would like to know if the audio is actually working on this board at all.....

Thanks

KVVD

This topic has been closed for replies.