Skip to main content
jaylong
Associate II
September 10, 2019
Solved

BlueNRG-2 5.0 long range support via lower bit rate

  • September 10, 2019
  • 3 replies
  • 986 views

Hi,

The BlueNRG-2 describes compatibility with the 5.0 spec. but I've been unable to find specific mention of the longer range via lower bit rate 500kbps or 125kbps and Forward Error Correction (FEC).

Is this long range mode supported and if so can you point me to some documentation?

Thanks!

jay

This topic has been closed for replies.
Best answer by Winfred LU

500 kbps and 125 kbps (coded PHY) is not supported for BlueNRG-2.

Thank you.

3 replies

Winfred LU
Winfred LUBest answer
ST Employee
September 11, 2019

500 kbps and 125 kbps (coded PHY) is not supported for BlueNRG-2.

Thank you.

jaylong
jaylongAuthor
Associate II
September 11, 2019

Thanks Winfred,

Do you know if there are any plans to enable this feature through firmware updates?

Thanks

jay

Winfred LU
ST Employee
September 12, 2019

Hi Jay,

Hardware modification is required to support the LE coded PHY.

The plan is to support both of them in the next generation of BlueNRG SoC : BlueNRG-LP, which is expected to be ready this year.

Best Regards,

Winfred