STM32H750 System Memory Bootloader Does Not Respond as App Notes AN2606 and AN3155 Suggests It Should
Hello!
A number of things to digest here:
The STM32 microcontroller system memory bootloader has not been responding correctly to my commands:
According to App note AN3155, I should be able to send a 0x7F to the serial port configured for booting as defined in app note AN2606. The problem is that I get a 0xA0 or other gibberish returned when I send that value out ranging from bauds of 9600 to 115200.
We have a stm32h750 with boot pins configured for USART2 rx and tx mapped to PA3 and PA2.
I realize in App note AN2606 on page 219 it states USART2 does not work for V13.2 but i have no way of identifying what version we are running, as the bootloader does not respond.
I assume my problem may be USART2, but the real question is, have I overlooked something? Also, is there a way to update the system memory bootloader? It would be nice to guarantee a fully working version of the bootloader for production purposes.
I eagerly await your response.
Thanks in advance,
Eric