Skip to main content
xxuej
Associate
September 10, 2019
Question

why my lis3dh current consume is bigger than spec?

  • September 10, 2019
  • 2 replies
  • 1137 views

​1 :

i only use the Lis3dh ,and remove all other elements

2: i use the power 3.0V, i use multimeter test the current consume between VCC and GND

get the test result current is 16 μA,

(the spec says ,the device automatically enters power-down mode, and current is 0.5μA)​

3, then i add the R1,it used for wake up the MCU,and connect to Lis3dh int 1 port ,

then a test the current like before ,but get the current is 56​μA, it is beyond my imagination .

so i want to ask ,is there anything wrong ?why i cannot get the power down mode current consume like spec says ?

0690X00000AQwXKQA1.png

This topic has been closed for replies.

2 replies

xxuej
xxuejAuthor
Associate
September 10, 2019

who can help me and give me reply ?​

ameeruak
Associate
January 8, 2020

Bump.

Seriously this is a really major issue and till now I have been unable to find a proper solution to it......

One solution the guy claims is here but that has not worked for me.

https://forums.adafruit.com/viewtopic.php?f=19&t=107822

I hope someone for ST can step in.