Skip to main content
svraj
Associate II
September 9, 2019
Solved

input capture problem in coding

  • September 9, 2019
  • 2 replies
  • 1059 views

Hi friends, i am capturing frequency using timer pins(Input capture mode).

MCU = stm32f103c8t6

Software = Keil uvision 5

Debugger = st-link v2

  • I capture frq using timer 1 ( TIM1_CC_IRQn ) channel 1 which is A8, which works awesome.
  • I tried similarly with timer 2 ( TIM2_IRQn ) channel 1 which is A0, which is also capture frequency well. But sticks into the TIM2_IRQHandler. My program execution is like, first it completes the main function, then it goes to TIM2_IRQHandler function, then its not returning back to while loop. It sticks inside the TIM2_IRQHandler function, whether it i apply frequency to the pin or not.

I am getting this issue only when i use other timers except timer 1.

code is given below (Register level language)...

#include "stm32f10x.h"
 
int main()
{
RCC->APB1ENR |=RCC_APB1ENR_TIM2EN;
 
	TIM2->PSC=7199;
	TIM2->CCMR1 |=TIM_CCMR1_CC1S_0; // set T2[1] as input capture
	TIM2->CCER &=~TIM_CCER_CC1P; // Rising edge
	TIM2->CCMR1 &=~TIM_CCMR1_IC1PSC; // Diabling the PSC
	TIM2->DIER |=TIM_DIER_UIE|TIM_DIER_CC1IE;
	TIM2->CCER |=TIM_CCER_CC1E;
	TIM2->CR1 |= TIM_CR1_CEN;
	NVIC_EnableIRQ(TIM2_IRQn);
 
while(1)
{
// Not entering to while loop??
}
}
 
 
// Interrupt handler
void TIM2_IRQHandler(void)
{ 
 
	if ((TIM2->SR & TIM_SR_CC1IF) != 0)
{
 if ((TIM2->SR & TIM_SR_CC1OF) != 0) /* Check the overflow */
 {
 /* Overflow error management */
 gap = 0; /* Reinitialize the laps computing */
 TIM2->SR &= ~(TIM_SR_CC1OF | TIM_SR_CC1IF); /* Clear the flags */
 } 
 if (gap == 0) /* Test if it is the first rising edge */
 {
	
 counter0 = TIM2->CCR1; /* Read the capture counter which clears the
 CC1ICF */
		
	 
 gap = 1; /* Indicate that the first rising edge has yet been detected */
 }
 else
 {
 counter1 = TIM2->CCR1; /* Read the capture counter which clears the
 CC1ICF */
	 
 if (counter1 > counter0) /* Check capture counter overflow */
 {
 Counter = counter1 - counter0;
	Frequency=10000/Counter; 
	 RPM=(Frequency*60)/4;
 }
 else
 {
 Counter = counter1 + 0xFFFF - counter0 + 1;
	 	Frequency=10000/Counter; 
			 RPM=(Frequency*60)/4;
 
 }
 counter0 = counter1; 
 }
}
else
{
 /* Unexpected Interrupt */	
 /* Manage an error for robust application */
} 
 
}

I think there is a mistake in my code in interrupt handler, kindly guide me friends to solve the issue.

This topic has been closed for replies.
Best answer by waclawek.jan

You enable Update Interrupt

TIM2->DIER |=TIM_DIER_UIE|TIM_DIER_CC1IE;

but you then don't manage it (clear its flag) in the ISR.

JW

2 replies

waclawek.jan
waclawek.janBest answer
Super User
September 9, 2019

You enable Update Interrupt

TIM2->DIER |=TIM_DIER_UIE|TIM_DIER_CC1IE;

but you then don't manage it (clear its flag) in the ISR.

JW

svraj
svrajAuthor
Associate II
September 11, 2019

Thank you waclawek, rightly spot

After clearing the flag it works fine.