Skip to main content
mal h
Associate II
Sep 8, 2019 2:46 PM UTC
Solved

IIS328DQ WHO_AM_I return not 0x32

Hi, I am using IIS328DQ with SPI communication. When I Check register WHO_AM_I, it was return 0x64. It is wrong because in datasheet it mention must be 0x32. So what is the solution?

Thanks​

This topic has been closed for replies.
Tesla DeLorean
Tesla DeLoreanBest answer
Guru
Sep 8, 2019 3:17 PM UTC

Check the clock/data phase settings, you are reading with a bit shift.​

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..

4 replies

Tesla DeLorean
Tesla DeLoreanBest answer
Guru
Sep 8, 2019 3:17 PM UTC

Check the clock/data phase settings, you are reading with a bit shift.​

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
mal h
mal hAuthor
Associate II
Sep 8, 2019 3:51 PM UTC

i think my configuration for SPI already match with spec in Datasheet sensor.

here my SPI configuration

 hspi1.Instance = SPI1;

 hspi1.Init.Mode = SPI_MODE_MASTER;

 hspi1.Init.Direction = SPI_DIRECTION_2LINES;

 hspi1.Init.DataSize = SPI_DATASIZE_8BIT;

 hspi1.Init.CLKPolarity = SPI_POLARITY_LOW;

 hspi1.Init.CLKPhase = SPI_PHASE_1EDGE;

 hspi1.Init.NSS = SPI_NSS_SOFT;

 hspi1.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_16;

 hspi1.Init.FirstBit = SPI_FIRSTBIT_MSB;

 hspi1.Init.TIMode = SPI_TIMODE_DISABLE;

 hspi1.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLE;

 hspi1.Init.CRCPolynomial = 0x0;

 hspi1.Init.NSSPMode = SPI_NSS_PULSE_ENABLE;

 hspi1.Init.NSSPolarity = SPI_NSS_POLARITY_LOW;

 hspi1.Init.FifoThreshold = SPI_FIFO_THRESHOLD_01DATA;

 hspi1.Init.TxCRCInitializationPattern = SPI_CRC_INITIALIZATION_ALL_ZERO_PATTERN;

 hspi1.Init.RxCRCInitializationPattern = SPI_CRC_INITIALIZATION_ALL_ZERO_PATTERN;

 hspi1.Init.MasterSSIdleness = SPI_MASTER_SS_IDLENESS_00CYCLE;

 hspi1.Init.MasterInterDataIdleness = SPI_MASTER_INTERDATA_IDLENESS_00CYCLE;

 hspi1.Init.MasterReceiverAutoSusp = SPI_MASTER_RX_AUTOSUSP_DISABLE;

 hspi1.Init.MasterKeepIOState = SPI_MASTER_KEEP_IO_STATE_DISABLE;

 hspi1.Init.IOSwap = SPI_IO_SWAP_DISABLE;

any suggestion?

Thanks

RNata.15
Associate II
Sep 11, 2019 2:24 PM UTC

HEY Muhammad , can you share your code on how you read