Skip to main content
Luis Ber
Associate II
September 4, 2019
Question

Is there a way to connect two STM32 through Ethernet (using a hub or multiplexer?)

  • September 4, 2019
  • 1 reply
  • 1285 views

Hello,

I'm doing a project where two microcontrollers (maybe one STM32H7 and STM32F7) must be connected between them. These two microcontrollers should be connected to an external Ethernet port.

Is there some type of hub or multiplexer that allows this type of connection? In the following lines I attach a image where I show the connection diagram:

0690X00000AQlcnQAD.png

Thank you in advance!

This topic has been closed for replies.

1 reply

Tesla DeLorean
Guru
September 4, 2019

There are certainly ethernet switch/hub devices that would achieve that either directly as a PHY, or through a PHY+Magnetics.

Not really my use case, you'd need to do your own research, due-diligence and prototyping here to determine the viability and code the drivers.

Would imagine chips by the like of Micrel and Realtek fit the bill.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..