cancel
Showing results for 
Search instead for 
Did you mean: 

Is it possible to install Raspbian on the STM32MP1 ? This is in order for example to interface the FLIR Lepton with it.

RogerPaudex
Associate II

See here

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
OlivierK
ST Employee

​Hello RogerPaudex (Flybotix),

At this time we only support our own OpenSTLinux s/w distribution, therefore at present Raspbian won't run on the STM32MP1as is.

You will need to customize your project to interface with the FLIR camera sensor, to interface with the SPI and I2C ports (STM32CubeMx can do that, in addition with the device tree generation) as well as application examples in STM32Cube_FW_MP1 library for SPI and I2C use.

I hope it helps.

Best Regards,

Olivier


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.