Skip to main content
Zui
Senior
August 29, 2019
Question

stm32h750 & IAR (EWARM)

  • August 29, 2019
  • 4 replies
  • 1017 views

Hello

I'm working with the stm32h750 eval board and touchgfx, my GUI is ready, but now i need to conect to some hardware (relay, sensors etc). i usually work with keil, but touchgfx not generating keil project and i lost hope it will before my dead-end; so i moved to IAR, which is generated, but not working, seems to me all options for the generated project are wrong, after many attempt (some random, some *** grano salis) i was able to compile a project, but still not able to load it into board (IAR starts to load project, and keeps going forever, no error, nothing, and i waited 40 min to see if it will eventually unstuck and load the code)

any advice/guide/working example to load touchGFX project from IAR?

Thanks

This topic has been closed for replies.

4 replies

Mike_ST
ST Technical Moderator
August 29, 2019

The code not loading into target most of the time, means that your project's options are wrong, especially debugger/ST-LINK options.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. 
Ozone
Principal
August 29, 2019

I would check IARs documentation, especially about the state of H7 support of their toolchain.

Flash/debug support and Flash loaders are the next thing to check.

Perhaps contacting IAR. They don't seem to have their own forum, though.

Working with IAR WB for Cortex M3/M4 MCUs myself (V7.30), never had such issues.

Tesla DeLorean
Guru
August 29, 2019

Presumably here a crap-tonne of data is being downloaded on to an external QSPI memory over the JTAG link.

Using a fast debug pod with USB 2.0 HS connection?

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Martin KJELDSEN
Principal III
September 6, 2019

How did you create this project? TouchGFX designer only has a complete package for H750-DISCO. Maybe you adapted an application based on that?

/Martin