Skip to main content
csinu
Associate II
August 27, 2019
Solved

STM32G4,Set Chip Read Protect,then can not connect the Chip。(had solved)

  • August 27, 2019
  • 5 replies
  • 1494 views

I used STM32CubeProgrammer,And Set Chip Read Protection(RDP:0xCC),

Now The Chip can not be connect By JLINK STLINK either Usart�?

is there some method to reset the protection level?

the problem had be solved,detail below:

Level 2: No debug

In this level, the protection level 1 is guaranteed. In addition, the Cortex®-M4 debug port, the

boot from RAM (boot RAM mode) and the boot from System memory (boot loader mode)

are no more available. In user execution mode (boot FLASH mode), all operations are

allowed on the Flash Main memory. On the contrary, only read operations can be performed

on the option bytes.

This topic has been closed for replies.
Best answer by Bob S

Time for a new chip unless your code already in the chip has a way to update itself. As I mentioned here

https://community.st.com/s/question/0D50X0000BFx3rSSQR/this-question-about-sbsfu-software-package-from-st-official-websiteand-i-download-the-sbsfu-package-to-my-stm32f413i-find-the-jtag-hw-interface-is-forbidden-how-can-i-do-to-download-other-programmer

Once you set RDP level 2 there is no going back. All JTAG/SWI access to FLASH and option bytes is blocked. The statement "in user execution mode ... all operations are allowed on the FLASH" means that the program running in the CPU can read, erase and program FLASH. But no external access is allowed.

5 replies

Bob S
Bob SBest answer
Super User
August 27, 2019

Time for a new chip unless your code already in the chip has a way to update itself. As I mentioned here

https://community.st.com/s/question/0D50X0000BFx3rSSQR/this-question-about-sbsfu-software-package-from-st-official-websiteand-i-download-the-sbsfu-package-to-my-stm32f413i-find-the-jtag-hw-interface-is-forbidden-how-can-i-do-to-download-other-programmer

Once you set RDP level 2 there is no going back. All JTAG/SWI access to FLASH and option bytes is blocked. The statement "in user execution mode ... all operations are allowed on the FLASH" means that the program running in the CPU can read, erase and program FLASH. But no external access is allowed.

Amel NASRI
ST Technical Moderator
August 29, 2019

Hi @csinu​ ,

Could you please tell us how your problem was solved?

-Amel

To give better visibility on the answered topics, please click on "Best Answer" on the reply which solved your issue or answered your question.
csinu
csinuAuthor
Associate II
August 29, 2019

@Amel NASRI (ST Employee)

Yes,My problem was solved。thank you,and thanks ST�?�?

Do I need to mark the problem was solved on this page?

Amel NASRI
ST Technical Moderator
August 29, 2019

@csinu​ ,

Glad to know that your problem was resolved. The more important is to share the solution with other members. In fact, someone else may face the same issue and your solution will be helpful for him.

If in this case the proposal of @Bob S​  was the solution for you, just click on "Select as Best" :)

-Amel

To give better visibility on the answered topics, please click on "Best Answer" on the reply which solved your issue or answered your question.
csinu
csinuAuthor
Associate II
August 29, 2019

@Amel NASRI (ST Employee)

I find Community is good for us(learner and engineer)。

when i public a question,and i can get the answer next day�?�?​haha