Question
Different return paths for STPM33 ICs?
Hello all,
Since i was not able to find thread for Power Monitoring ICs, hence, posting my question here.
I am using STPM33 PM IC for my application and i have below queries:-
- As i can see in the datasheet in the application schematic column, two ground references are used: One for Analog ground and the other for digital ground. And also, these two ground paths are shorted. Screenshot below:-

Kindly let me know the advantages of doing it this way and not having a single ground reference.
- Does this STPM33 IC work as a slave or master when configured over SPI?
- I am planning to use 8xSTPM33 device configured over SPI on a single SPI bus with different CS lines dedicated for each STPM33 IC. The SPI master is supposed to be STM32L452RCT6 MCU.
- Since i am using multiple STPM33 ICs, we need to calibrate them. Thus should i have an extra EEPROM on my board for storing these calibration values? or can i do something like this with my MCU. Kindly direct me towards an application note, if any, about this. I have an SD card provision on my board. Can i do calibration using it? If yes, please let me know for its application note.
Thanks a lot in advance. Waiting for a positive reply.
Have a nice day!
Best Regards,
Yash