Question
I2C Reception Issue with DMA in HAL Library
Hello
I am implementing I2C transfer with DMA in stm32.
Processor: stm32l152rdt6
DMA Configuration:
I would like to continuously receive 3 bytes from master, so I use circular mode.

NVIC Configuration:

I2C Initialization Code:
hi2c1.Instance = I2C1;
hi2c1.Init.ClockSpeed = 400000;
hi2c1.Init.DutyCycle = I2C_DUTYCYCLE_2;
hi2c1.Init.OwnAddress1 = I2C_ADDRESS*2;
hi2c1.Init.AddressingMode = I2C_ADDRESSINGMODE_7BIT;
hi2c1.Init.DualAddressMode = I2C_DUALADDRESS_DISABLE;
hi2c1.Init.OwnAddress2 = 0;
hi2c1.Init.GeneralCallMode = I2C_GENERALCALL_DISABLE;
hi2c1.Init.NoStretchMode = I2C_NOSTRETCH_DISABLE;
if (HAL_I2C_Init(&hi2c1) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN I2C1_Init 2 */
HAL_I2C_Slave_Receive_DMA( &hi2c1, ucRxbuffer_obc, 3);I use HAL_I2C_SlaveRxCpltCallback to check transfer condition.
However, it seems the callback function only triggered in first time.
void HAL_I2C_SlaveRxCpltCallback(I2C_HandleTypeDef *hi2c)
{
if(hi2c->Instance == I2C1)
{
sprintf(cMessage, "message[0]: %u\n\r", ucRxbuffer_obc[0]);
debugprintf(cMessage);
}
}I trace the condition and I found DMA state of RX kept busy but I have no idea how to deal with it.
Is there anything I miss?