Skip to main content
ASeyo
Associate II
August 22, 2019
Solved

I2C start condition not generates ( SB flag is never set )

  • August 22, 2019
  • 2 replies
  • 2172 views

I'm working on stm32f103 I2C peripheral. I've one stm32f103 master and another stm32f103 slave. The master should send some text to the slave, but start condition never generates. The BUSY flag is set as soon as the peripheral is enable and the program hangs on a loop that waits until start condition is generated.

( i.e
 // Wait until start condition is generated
	while(!(I2C1->SR1 & I2C_SR1_S){}
)
 
#include "stm32f10x.h" // Device header
void clockConfig(void);
void I2C1Init(void);
void I2C1Send(uint8_t* MSG);
int main(void)
{
	clockConfig();
	I2C1Init();
	I2C1Send((uint8_t*)"Hello, I2C1!");
while(1)
	{
	}
}
 
void I2C1Send(uint8_t* MSG)
{
	// Generate start bit
	I2C1->CR1 |= I2C_CR1_START;
	// Wait until start condition is generated
	while(!(I2C1->SR1 & I2C_SR1_SB)){} /* the program stops here*/
	// clear start condition flag
	uint32_t dummyRead = I2C1->SR1;
	// Write slave address, and master transmitter mode
	I2C1->DR = 0x72; 
	// Wait until address phase is complete
	while(!(I2C1->SR1 & I2C_SR1_ADDR)){}
	// Clear ADDR
 dummyRead = I2C1->SR1;
	dummyRead = I2C1->SR2;	
 
	while(*MSG)
	{
 
 // Wait until TXE flag is set
 while(!(I2C1->SR1 & I2C_SR1_TXE)){}
 I2C1->DR = *MSG;
 MSG++;
	}
 
	// Wait unitl byte trasfer finished flag
	while(!(I2C1->SR1 & I2C_SR1_BTF)){}
	// program stop condition
	I2C1->CR1 |= I2C_CR1_STOP;
	// BTF flag is cleared by hardware 
 
}
 
void I2C1Init(void)
{	
	// Enable clock access for port B
	RCC->APB2ENR |= RCC_APB2ENR_IOPBEN;
 
	// Configure Gpios as af open drain
	GPIOB->CRL |= GPIO_CRL_CNF6 | GPIO_CRL_MODE6;
	// Enable internal pull up
	GPIOB->ODR |= GPIO_ODR_ODR6;
	GPIOB->CRL |= GPIO_CRL_CNF7 | GPIO_CRL_MODE7;
	// Enable internal pull up
	GPIOB->ODR |= GPIO_ODR_ODR7;
	// Configure I2C1
	// Enable clock access for I2C1
	RCC->APB1ENR |= RCC_APB1ENR_I2C1EN;
	// Configure APB1 frequency
	I2C1->CR2 |= 36;
	// configure CCR
	I2C1->CCR |= 180; // 100KHz standard mode
	// Configure the rise time register
	I2C1->TRISE |= 37;
	// Enable I2C1
	I2C1->CR1 |= I2C_CR1_PE;
	// Enable ACK 
	I2C1->CR1 |= I2C_CR1_ACK;	
}
 
 /* This sets all peripherals to their maximum speed.*/
void clockConfig(void)
{
	// HSE ON
	RCC->CR |= 0x1<<16;
 // wait unit HSE is ready
	while(!(RCC->CR & (0x1<<17))){}
 
	// PLL OFF
	RCC->CR &= ~(0x1<<24);
	//HSE clock not divided
	RCC->CFGR &= ~(0x1<<17);
	// PLL SRC = HSE 
	RCC->CFGR |= 0x1<<16;
	// PLL MUL, x9
	RCC->CFGR &= ~(0xF<<18);
	RCC->CFGR |= 0x7<<18;
 
 	// PLL ON
	RCC->CR |= 0x1<<24;
	// wait until PLL is ready
	while(!(RCC->CR & (0x1 << 25))){}
 
	// choose PLL as Sys clock 
	RCC->CFGR &= ~(0x3);
	RCC->CFGR |= 0x2;
 
	// AHB prescaler x1
	RCC->CFGR &= ~(0xF<<4);
	
 // APB1 (36MHz max ) prescaler /2
	RCC->CFGR &= ~(0x7<<8);
	RCC->CFGR |= (0x4<<8);
 
 // APB2(72MHz) prescaler x1
	RCC->CFGR &= ~(0x7<<11);
}

This topic has been closed for replies.
Best answer by Amel NASRI

Hi @ASeyo​ ,

Please make sure that the sequence recommended in the product errata sheet (I2C analog filter may provide wrong value, locking BUSY flag and preventing master mode entry) is well applied.

Here the link to the errata sheet document.

-Amel

2 replies

Amel NASRI
Amel NASRIBest answer
ST Technical Moderator
August 22, 2019

Hi @ASeyo​ ,

Please make sure that the sequence recommended in the product errata sheet (I2C analog filter may provide wrong value, locking BUSY flag and preventing master mode entry) is well applied.

Here the link to the errata sheet document.

-Amel

To give better visibility on the answered topics, please click on "Best Answer" on the reply which solved your issue or answered your question.
Visitor II
May 7, 2024

Is there a sample mxcube generated code with errata applied?